<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic periph_sdmmc not working on LPC43s67 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/periph-sdmmc-not-working-on-LPC43s67/m-p/647424#M25671</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using LPC43s67 EVM Board, as per design requirement i have to use micro sd card with SDIO interface,&lt;/P&gt;&lt;P&gt;so in my custom design am using micro sd card connector PFA,&lt;/P&gt;&lt;P&gt;i am attaching connection i made for micro sd card,&lt;/P&gt;&lt;P&gt;confusing for me is that in LPCopen periph_sdmmc code DAT3 pin is assigned&amp;nbsp; to P1.12 and CD pin is assigned to P1.13,&lt;/P&gt;&lt;P&gt;but in my connection i can not use CD and DAT3 pin as it is a single pin coming from micro sd card,&lt;/P&gt;&lt;P&gt;so tried connecting CD/DAT3 pin on micro sd card to P1.13 of EVm Board but card is not getting detected,&lt;/P&gt;&lt;P&gt;i tried giving directly GND signal to P1.13 and CD/DAT3 pin of micro sd card to P1.12 of EVM Board ,&lt;/P&gt;&lt;P&gt;so here card acquire is getting failed,&lt;/P&gt;&lt;P&gt;is there any issue in periph_sdmmc or in my design or i have to change something,&lt;/P&gt;&lt;P&gt;i have attached all the related files,&lt;/P&gt;&lt;P&gt;please suggest it will be helpful for me,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jan 2017 14:06:33 GMT</pubDate>
    <dc:creator>sagarpatil</dc:creator>
    <dc:date>2017-01-26T14:06:33Z</dc:date>
    <item>
      <title>periph_sdmmc not working on LPC43s67</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/periph-sdmmc-not-working-on-LPC43s67/m-p/647424#M25671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using LPC43s67 EVM Board, as per design requirement i have to use micro sd card with SDIO interface,&lt;/P&gt;&lt;P&gt;so in my custom design am using micro sd card connector PFA,&lt;/P&gt;&lt;P&gt;i am attaching connection i made for micro sd card,&lt;/P&gt;&lt;P&gt;confusing for me is that in LPCopen periph_sdmmc code DAT3 pin is assigned&amp;nbsp; to P1.12 and CD pin is assigned to P1.13,&lt;/P&gt;&lt;P&gt;but in my connection i can not use CD and DAT3 pin as it is a single pin coming from micro sd card,&lt;/P&gt;&lt;P&gt;so tried connecting CD/DAT3 pin on micro sd card to P1.13 of EVm Board but card is not getting detected,&lt;/P&gt;&lt;P&gt;i tried giving directly GND signal to P1.13 and CD/DAT3 pin of micro sd card to P1.12 of EVM Board ,&lt;/P&gt;&lt;P&gt;so here card acquire is getting failed,&lt;/P&gt;&lt;P&gt;is there any issue in periph_sdmmc or in my design or i have to change something,&lt;/P&gt;&lt;P&gt;i have attached all the related files,&lt;/P&gt;&lt;P&gt;please suggest it will be helpful for me,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 14:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/periph-sdmmc-not-working-on-LPC43s67/m-p/647424#M25671</guid>
      <dc:creator>sagarpatil</dc:creator>
      <dc:date>2017-01-26T14:06:33Z</dc:date>
    </item>
  </channel>
</rss>