<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Apply LPCXpresso54608 for Vehicle positioning system based on image recognition</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Apply-LPCXpresso54608-for-Vehicle-positioning-system-based-on/m-p/647204#M25665</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in the development of&amp;nbsp;vehicle positioning system based on image recognition, within a certain space principle is through the multiple video signal to collect the captured image signal, through optical flow, distance analysis processing, fusion positioning the objects being measured the three-dimensional coordinates of points in space, and calculate the movement direction, speed and acceleration of the object, upload the first machine. Project image algorithm part and upper machine part has been completed, but high performance processors are needed as carrying platform, therefore, I apply for this activity's LPCXpresso54608 development board.&lt;/P&gt;&lt;P&gt;I hope LPCXpresso54608, such a high-performance processor with Cortex-M4 kernel of can do perfect in my design,and thanks to NXP community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Dec 2016 10:08:40 GMT</pubDate>
    <dc:creator>jianghaoyu</dc:creator>
    <dc:date>2016-12-28T10:08:40Z</dc:date>
    <item>
      <title>Apply LPCXpresso54608 for Vehicle positioning system based on image recognition</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Apply-LPCXpresso54608-for-Vehicle-positioning-system-based-on/m-p/647204#M25665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in the development of&amp;nbsp;vehicle positioning system based on image recognition, within a certain space principle is through the multiple video signal to collect the captured image signal, through optical flow, distance analysis processing, fusion positioning the objects being measured the three-dimensional coordinates of points in space, and calculate the movement direction, speed and acceleration of the object, upload the first machine. Project image algorithm part and upper machine part has been completed, but high performance processors are needed as carrying platform, therefore, I apply for this activity's LPCXpresso54608 development board.&lt;/P&gt;&lt;P&gt;I hope LPCXpresso54608, such a high-performance processor with Cortex-M4 kernel of can do perfect in my design,and thanks to NXP community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 10:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Apply-LPCXpresso54608-for-Vehicle-positioning-system-based-on/m-p/647204#M25665</guid>
      <dc:creator>jianghaoyu</dc:creator>
      <dc:date>2016-12-28T10:08:40Z</dc:date>
    </item>
  </channel>
</rss>