<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SSP0 Receive FIFO in LPC11U68J100 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647015#M25638</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ladies and gentlemen,&lt;/P&gt;&lt;P&gt;nobody knows the answer of these questions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Nov 2016 07:35:01 GMT</pubDate>
    <dc:creator>jeanvaljean</dc:creator>
    <dc:date>2016-11-03T07:35:01Z</dc:date>
    <item>
      <title>SSP0 Receive FIFO in LPC11U68J100</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647014#M25637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Gentlemen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it possible to see somehow in LPCXpresso the receive FIFO of LPC11U68J100 controller?&lt;/P&gt;&lt;P&gt;I'd like to check it, because I don't have the same data in SSP0_DR&amp;nbsp; what the master sends. The uC is configured as slave. I got the SSP0 interrupt, something comes in but not what I expect.&lt;/P&gt;&lt;P&gt;Signals are checked by oscilloscope, they're correct. I should have some SW issue there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case my uC is slave, should the internal SSP0 clock have exactly the same frequency, as the master has?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chip is on OM13058 LPCXpresso board, I use LPCXpresso 8.1.4 on Win7.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 13:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647014#M25637</guid>
      <dc:creator>jeanvaljean</dc:creator>
      <dc:date>2016-10-18T13:02:25Z</dc:date>
    </item>
    <item>
      <title>Re: SSP0 Receive FIFO in LPC11U68J100</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647015#M25638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ladies and gentlemen,&lt;/P&gt;&lt;P&gt;nobody knows the answer of these questions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 07:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647015#M25638</guid>
      <dc:creator>jeanvaljean</dc:creator>
      <dc:date>2016-11-03T07:35:01Z</dc:date>
    </item>
    <item>
      <title>Re: SSP0 Receive FIFO in LPC11U68J100</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647016#M25639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Peripheral View should&amp;nbsp;give you access to the Status Register (which will tell you if the FIFO is empty or full), &amp;nbsp;but I don't think this will give you access to the actual FIFO itself (unless it is exposed in the memory map).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might get more focused advice from the LPC community (for hardware usage) rather than the LPCXpresso IDE one - which is focussed more on tools usage. So I'll transfer your question there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 08:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP0-Receive-FIFO-in-LPC11U68J100/m-p/647016#M25639</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-11-03T08:17:57Z</dc:date>
    </item>
  </channel>
</rss>