<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: ADCHS LPC4370 Problems creation interface.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645795#M25531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Vin(range) is only suitable for differential mode , which doesn't applicable to single ended ADC configuration.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Feb 2017 08:36:27 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-02-21T08:36:27Z</dc:date>
    <item>
      <title>ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645792#M25528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;good morning,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We are undertaking a project with the micro lpc3470 and we find it difficult to properly size the interface circuit for the analog readings by adchs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use the internal vref to 0.5V, in the datasheet is reported that the range of values are compared -400mV to + vref. But in the datasheet lpc3470 page. 131&lt;/P&gt;&lt;P&gt;Symbol Parameter Conditions Min Typ Max Unit&lt;/P&gt;&lt;P&gt;VDC DC input common mode level 0.1 0.5 0.9 V&lt;BR /&gt;-2048 0 +2047 digit&lt;/P&gt;&lt;P&gt;We (range) input voltage peak-to-peak 0.72 0.8 0.88 V&lt;/P&gt;&lt;P&gt;The minimum value in this case may range from 0.1 to 0.14V?&lt;/P&gt;&lt;P&gt;The maximum value in this case can range from 0.86 to 0.94V?&lt;/P&gt;&lt;P&gt;We can not correctly interpret these data.&lt;/P&gt;&lt;P&gt;Can you help?&lt;/P&gt;&lt;P&gt;Thanks and good job&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 08:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645792#M25528</guid>
      <dc:creator>fabiodebernardi</dc:creator>
      <dc:date>2017-02-17T08:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645793#M25529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC4370 12-bit high speed ADC common mode is using internal vin_neg 0.5V reference voltage connects with ADCHS_NEG pin. The vin_pos should be in the range from 0.50 ± 0.4 V.&lt;/P&gt;&lt;P&gt;Customer could find below data from LPC4370 datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14663i958D47669FCD181C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When deselect the internal vin_neg and supply vin_neg externally at pin ADCHS_NEG by setting DCINNEG to 0. Then customer is using the ADC with differential mode.&lt;/P&gt;&lt;P&gt;So, customer need to refer below table about one of ADCHS_[0:5] input pin and ADCHS_NEG input voltage peak to peak range:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14800i328B86AB40817C58/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When ADC works in differential mode, the peak to peak typical value is 0.8V.&lt;/P&gt;&lt;P&gt;For example if the ADCHS_NEG input voltage is 0.7V, the ADCHS_0 pin input voltage could low to 0V and up to 1.2V (ADCHS module with Measurement range 0 to 1.2 V&amp;nbsp; feature).&lt;/P&gt;&lt;P&gt;The Vin(range) Min. value 0.72V and Max. value 0.88V are based on the test results. The typical value is 0.8V.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 07:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645793#M25529</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-02-21T07:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645794#M25530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;This last consideration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;"The Vin(range) Min. value 0.72V and Max. value 0.88V are based on the test results. The typical value is 0.8V."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;is it applicable to single ended ADC configuration?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 08:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645794#M25530</guid>
      <dc:creator>fabiodebernardi</dc:creator>
      <dc:date>2017-02-21T08:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645795#M25531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Vin(range) is only suitable for differential mode , which doesn't applicable to single ended ADC configuration.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 08:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645795#M25531</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-02-21T08:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645796#M25532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui_Ma,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;good job&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 09:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645796#M25532</guid>
      <dc:creator>fabiodebernardi</dc:creator>
      <dc:date>2017-02-21T09:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645797#M25533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" class="" data-userid="15678" data-username="Hui_Ma" href="https://community.nxp.com/people/Hui_Ma" style="color: #5e89c1; background-color: #ffffff; border: 0px; font-weight: 200; font-size: 1.286rem;"&gt;Hui&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean that we had to consider for single ended config. the range 0.1 to 0,9V without tolerance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THKS!&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 09:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645797#M25533</guid>
      <dc:creator>fabiodebernardi</dc:creator>
      <dc:date>2017-02-21T09:35:20Z</dc:date>
    </item>
    <item>
      <title>Re: ADCHS LPC4370 Problems creation interface.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645798#M25534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is based on customer application to determine which ADCHS mode will be used.&lt;/P&gt;&lt;P&gt;The range 0.1V to 0.9V single ended mode without tolerance (vin_pos should be in the range&lt;BR /&gt;from 0.50 ± 0.4 V ). &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 09:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADCHS-LPC4370-Problems-creation-interface/m-p/645798#M25534</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-02-21T09:48:55Z</dc:date>
    </item>
  </channel>
</rss>