<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Unable to read GPIO pin value using ReadPortbit and GetPinstate function despite setting Pindirection</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644913#M25514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using an LPC 43s67 evaluation board. I fixed the issue&lt;/P&gt;&lt;P&gt;The input buffer is disabled by default. So i enabled it using the scu config.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jan 2017 09:33:28 GMT</pubDate>
    <dc:creator>arvindprasad</dc:creator>
    <dc:date>2017-01-06T09:33:28Z</dc:date>
    <item>
      <title>Unable to read GPIO pin value using ReadPortbit and GetPinstate function despite setting Pindirection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644911#M25512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am unable to read the GPIO pin value. I have set the direction correctly, I have even tried setting another GPIO pin HIGH and connecting it to the input GPIO pin, but the readPortbit and GetPinstate function still returns a&amp;nbsp; zero.#GPIO lpc43sxx #GPIO read &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 03:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644911#M25512</guid>
      <dc:creator>arvindprasad</dc:creator>
      <dc:date>2016-12-28T03:52:54Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to read GPIO pin value using ReadPortbit and GetPinstate function despite setting Pindirection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644912#M25513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please let me know which device, board, IDE are you using?&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 15:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644912#M25513</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-12-28T15:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to read GPIO pin value using ReadPortbit and GetPinstate function despite setting Pindirection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644913#M25514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using an LPC 43s67 evaluation board. I fixed the issue&lt;/P&gt;&lt;P&gt;The input buffer is disabled by default. So i enabled it using the scu config.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 09:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-read-GPIO-pin-value-using-ReadPortbit-and-GetPinstate/m-p/644913#M25514</guid>
      <dc:creator>arvindprasad</dc:creator>
      <dc:date>2017-01-06T09:33:28Z</dc:date>
    </item>
  </channel>
</rss>