<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックhelp with LPCXpresso examples for LPC1114</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/help-with-LPCXpresso-examples-for-LPC1114/m-p/644738#M25500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to learn about the LPC1114, and is therefore using the lpcxpresso.examples.lpc1114.302.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the Blinky and the Uart examples, and both work perfectly, but i would like to combine them. &lt;BR /&gt;when trying to combine the two projects, i include the gpio.h and the timer32.h, and include the following lines of code in the main part of the program:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lines of code in main&lt;/P&gt;&lt;DIV&gt;- init_timer32(0, TIME_INTERVAL);&lt;/DIV&gt;&lt;DIV&gt;- enable_timer32(0);&lt;/DIV&gt;&lt;DIV&gt;- GPIOInit();&lt;/DIV&gt;&lt;DIV&gt;- GPIOSetValue( LED_PORT, LED_BIT, LED_OFF );&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building the program resoults in several errors. The errors are fx. "undefined reference to ´GPIOInit´".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that the drivers for the Uart example hilight the uart.h and uart.c amoungst others, but gpio.h and gpio.c are not highlighted, is this perhaps a part of the problem, and if this is the case how can it be fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 19:43:24 GMT</pubDate>
    <dc:creator>thomashavregaar</dc:creator>
    <dc:date>2017-04-26T19:43:24Z</dc:date>
    <item>
      <title>help with LPCXpresso examples for LPC1114</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/help-with-LPCXpresso-examples-for-LPC1114/m-p/644738#M25500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to learn about the LPC1114, and is therefore using the lpcxpresso.examples.lpc1114.302.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the Blinky and the Uart examples, and both work perfectly, but i would like to combine them. &lt;BR /&gt;when trying to combine the two projects, i include the gpio.h and the timer32.h, and include the following lines of code in the main part of the program:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lines of code in main&lt;/P&gt;&lt;DIV&gt;- init_timer32(0, TIME_INTERVAL);&lt;/DIV&gt;&lt;DIV&gt;- enable_timer32(0);&lt;/DIV&gt;&lt;DIV&gt;- GPIOInit();&lt;/DIV&gt;&lt;DIV&gt;- GPIOSetValue( LED_PORT, LED_BIT, LED_OFF );&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building the program resoults in several errors. The errors are fx. "undefined reference to ´GPIOInit´".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that the drivers for the Uart example hilight the uart.h and uart.c amoungst others, but gpio.h and gpio.c are not highlighted, is this perhaps a part of the problem, and if this is the case how can it be fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 19:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/help-with-LPCXpresso-examples-for-LPC1114/m-p/644738#M25500</guid>
      <dc:creator>thomashavregaar</dc:creator>
      <dc:date>2017-04-26T19:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: help with LPCXpresso examples for LPC1114</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/help-with-LPCXpresso-examples-for-LPC1114/m-p/644739#M25501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;I suppose there is a shortage of paths&lt;/SPAN&gt;&lt;/SPAN&gt; for include in project settings.&lt;/P&gt;&lt;P&gt;You must add path to gpio:&lt;/P&gt;&lt;P&gt;1. Settings&lt;/P&gt;&lt;P&gt;2. includes&lt;/P&gt;&lt;P&gt;3. click symbol Add..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after enter path to gpio.h&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="gpio_settings.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14246iFE0740A1C562470D/image-size/large?v=v2&amp;amp;px=999" role="button" title="gpio_settings.png" alt="gpio_settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 07:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/help-with-LPCXpresso-examples-for-LPC1114/m-p/644739#M25501</guid>
      <dc:creator>Badman</dc:creator>
      <dc:date>2017-04-27T07:50:09Z</dc:date>
    </item>
  </channel>
</rss>