<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Adding and reading of an binary file(.bin)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Adding-and-reading-of-an-binary-file-bin/m-p/643573#M25422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use the "incbin" assembler directive. See this post for more nfo&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/418385"&gt;https://community.nxp.com/thread/418385&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Mar 2017 16:33:50 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2017-03-13T16:33:50Z</dc:date>
    <item>
      <title>Adding and reading of an binary file(.bin)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Adding-and-reading-of-an-binary-file-bin/m-p/643572#M25421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using LPC54102 evaluation board and have imported a project in LPCXpresso_8.1.0_597 for send data via UART using LPC54102. I have a binary file(.bin) of other board which was created by keil IDE. My task is to send the content of that bin file to other board via UART communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions are&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How can i add this bin file into LPCXpresso project file ?&lt;/P&gt;&lt;P&gt;2. How can i combine this .bin file to create the single .axf( or .hex) file with linker ?&lt;/P&gt;&lt;P&gt;3. is there any way to complete this task ? (IAR compiler has an option to do this, i done this using IAR IDE )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please give your suggestion&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 13:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Adding-and-reading-of-an-binary-file-bin/m-p/643572#M25421</guid>
      <dc:creator>ratheesht</dc:creator>
      <dc:date>2017-03-13T13:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: Adding and reading of an binary file(.bin)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Adding-and-reading-of-an-binary-file-bin/m-p/643573#M25422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use the "incbin" assembler directive. See this post for more nfo&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/418385"&gt;https://community.nxp.com/thread/418385&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 16:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Adding-and-reading-of-an-binary-file-bin/m-p/643573#M25422</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-03-13T16:33:50Z</dc:date>
    </item>
  </channel>
</rss>