<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 initiation ethernet block lpc1768, target error 15</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/initiation-ethernet-block-lpc1768-target-error-15/m-p/642093#M25396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to initiate the Ethernet block on a lpc1768.&lt;/P&gt;&lt;P&gt;The block is powered up. The pins are set&lt;/P&gt;&lt;P&gt;EMAC-MAC1 reset is set and deasserted.&lt;/P&gt;&lt;P&gt;EMAC-Command reset set.&lt;/P&gt;&lt;P&gt;Next step is initialising MAC control registers.&lt;/P&gt;&lt;P&gt;EMAC-MAC1 = all pass flag set etc..&lt;/P&gt;&lt;P&gt;At this point&amp;nbsp; SW debug breaks down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;15: Target error from Register access: Ee(FF). Redlink interface error 255.&lt;/P&gt;&lt;P&gt;It is impossible to pass this point in the program. Whatever I skip in the rest of the program after reset of the MAC I either get this message or the program gets somewhere in loop.&lt;/P&gt;&lt;P&gt;When I stop the debug. It takes some time before the IDE responds with terminating the process all together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Who has a solution?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Mar 2017 10:06:28 GMT</pubDate>
    <dc:creator>martinbal</dc:creator>
    <dc:date>2017-03-10T10:06:28Z</dc:date>
    <item>
      <title>initiation ethernet block lpc1768, target error 15</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/initiation-ethernet-block-lpc1768-target-error-15/m-p/642093#M25396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to initiate the Ethernet block on a lpc1768.&lt;/P&gt;&lt;P&gt;The block is powered up. The pins are set&lt;/P&gt;&lt;P&gt;EMAC-MAC1 reset is set and deasserted.&lt;/P&gt;&lt;P&gt;EMAC-Command reset set.&lt;/P&gt;&lt;P&gt;Next step is initialising MAC control registers.&lt;/P&gt;&lt;P&gt;EMAC-MAC1 = all pass flag set etc..&lt;/P&gt;&lt;P&gt;At this point&amp;nbsp; SW debug breaks down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;15: Target error from Register access: Ee(FF). Redlink interface error 255.&lt;/P&gt;&lt;P&gt;It is impossible to pass this point in the program. Whatever I skip in the rest of the program after reset of the MAC I either get this message or the program gets somewhere in loop.&lt;/P&gt;&lt;P&gt;When I stop the debug. It takes some time before the IDE responds with terminating the process all together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Who has a solution?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Mar 2017 10:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/initiation-ethernet-block-lpc1768-target-error-15/m-p/642093#M25396</guid>
      <dc:creator>martinbal</dc:creator>
      <dc:date>2017-03-10T10:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: initiation ethernet block lpc1768, target error 15</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/initiation-ethernet-block-lpc1768-target-error-15/m-p/642094#M25397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem lies in a not working PHY chip. During initiation of the Ethernet block nearly immediately an internal communication&amp;nbsp; between ethernet block and PHY takes place. Because the PHY is not reacting, It results in an internal wait state. The debuffer has not access to this process. &lt;/P&gt;&lt;P&gt;With a proper functioning PHY chip the communicion finishes properly&amp;nbsp; and control is returned to the flash code. At that point the debugger can follow the execution again.&lt;/P&gt;&lt;P&gt;Problem solved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Mar 2017 11:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/initiation-ethernet-block-lpc1768-target-error-15/m-p/642094#M25397</guid>
      <dc:creator>martinbal</dc:creator>
      <dc:date>2017-03-12T11:47:55Z</dc:date>
    </item>
  </channel>
</rss>