<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Why disconnected USB cable blocks running code ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641961#M25395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;As the &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="290358" data-username="converse" href="https://community.nxp.com/people/converse"&gt;Con Verse&lt;/A&gt;&lt;/SPAN&gt; mentioned, it needs to use a debugger to figure out the root cause of the issue.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 02:15:05 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-12-29T02:15:05Z</dc:date>
    <item>
      <title>Why disconnected USB cable blocks running code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641958#M25392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I use LPC11U35 on my board and it is powered by battery. It is developed under mbed.org platform and I have a problem with USBSerial (USB CDC). The board works fine with connected USB cable or without USB cable. The problem is when I disconnect USB cable from running board because then running code is stoped. I do not know where is problem. Is it a problem with mbed library or is it a hardware problem ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 01:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641958#M25392</guid>
      <dc:creator>peteraugustin</dc:creator>
      <dc:date>2016-12-27T01:20:25Z</dc:date>
    </item>
    <item>
      <title>Re: Why disconnected USB cable blocks running code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641959#M25393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably a problem with your code... Some suggestions:&lt;/P&gt;&lt;P&gt;- removing the power causes a dip in power that is detected as a brown-out, and you have a handler&lt;/P&gt;&lt;P&gt;- there is a USB interrupt dfor device removal that is not being handled&lt;/P&gt;&lt;P&gt;- there is a fault being generated&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whatever the problem, you will need to use a debugger to find the cause&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 09:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641959#M25393</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2016-12-27T09:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Why disconnected USB cable blocks running code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641960#M25394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Thanks for your answer. One more thing, when I turn off my PC by standard shutdown process with connected USB cable then the problem does not Occur and the code continues.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 10:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641960#M25394</guid>
      <dc:creator>peteraugustin</dc:creator>
      <dc:date>2016-12-27T10:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: Why disconnected USB cable blocks running code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641961#M25395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;As the &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="290358" data-username="converse" href="https://community.nxp.com/people/converse"&gt;Con Verse&lt;/A&gt;&lt;/SPAN&gt; mentioned, it needs to use a debugger to figure out the root cause of the issue.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 02:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Why-disconnected-USB-cable-blocks-running-code/m-p/641961#M25395</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-29T02:15:05Z</dc:date>
    </item>
  </channel>
</rss>