<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC1758 Proper way to disable/re-enable USB endpoint while DMA transfer is queued</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Proper-way-to-disable-re-enable-USB-endpoint-while-DMA/m-p/641361#M25364</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having an issue where if a USB DMA transfer is queued and the endpoint is disabled and then re-enabled (using the SIE interface), the DMA descriptor will be retired but no EOT or Error interrupt will be raised.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there way to cancel a DMA transfer without waiting for it to complete?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 06:43:53 GMT</pubDate>
    <dc:creator>james3434</dc:creator>
    <dc:date>2016-09-22T06:43:53Z</dc:date>
    <item>
      <title>LPC1758 Proper way to disable/re-enable USB endpoint while DMA transfer is queued</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Proper-way-to-disable-re-enable-USB-endpoint-while-DMA/m-p/641361#M25364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having an issue where if a USB DMA transfer is queued and the endpoint is disabled and then re-enabled (using the SIE interface), the DMA descriptor will be retired but no EOT or Error interrupt will be raised.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there way to cancel a DMA transfer without waiting for it to complete?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 06:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Proper-way-to-disable-re-enable-USB-endpoint-while-DMA/m-p/641361#M25364</guid>
      <dc:creator>james3434</dc:creator>
      <dc:date>2016-09-22T06:43:53Z</dc:date>
    </item>
  </channel>
</rss>