<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Need to declare variables in external SDRAM  as well in the internal RAM.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640153#M25311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill,&lt;/P&gt;&lt;P&gt;You could take a look at the following links, which seems to be related to what are you trying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram"&gt;https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/could-i-use-extern-sdram-ram"&gt;https://www.lpcware.com/content/forum/could-i-use-extern-sdram-ram&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/429937"&gt;https://community.nxp.com/thread/429937&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jan 2017 19:41:40 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2017-01-04T19:41:40Z</dc:date>
    <item>
      <title>Need to declare variables in external SDRAM  as well in the internal RAM.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640152#M25310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using an LPC2468 processor with external SDRAM&amp;nbsp;starting at address 0xa000000 in addition to the the processors built in RAM. &amp;nbsp;I am using Kiel uVision. &amp;nbsp;I need to define variables in both address spaces. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to define each variable using the __attribute__ modifier? &amp;nbsp;If so, how?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to say, from here until I say otherwise use this memory space or the other ? &amp;nbsp;Or does each variable need its own qualifier? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have played with the scatter allocation file but looking at the map file variables are still allocated in unexpected places/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Dec 2016 03:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640152#M25310</guid>
      <dc:creator>billbrown</dc:creator>
      <dc:date>2016-12-25T03:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: Need to declare variables in external SDRAM  as well in the internal RAM.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640153#M25311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill,&lt;/P&gt;&lt;P&gt;You could take a look at the following links, which seems to be related to what are you trying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram"&gt;https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/could-i-use-extern-sdram-ram"&gt;https://www.lpcware.com/content/forum/could-i-use-extern-sdram-ram&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/429937"&gt;https://community.nxp.com/thread/429937&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 19:41:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640153#M25311</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-01-04T19:41:40Z</dc:date>
    </item>
    <item>
      <title>Re: Need to declare variables in external SDRAM  as well in the internal RAM.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640154#M25312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kiel docs how to do this&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.keil.com/support/docs/2829.htm" title="http://www.keil.com/support/docs/2829.htm"&gt;ARM: LOCATING VARIABLES AT ABSOLUTE MEMORY ADDRESSES&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 12:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-declare-variables-in-external-SDRAM-as-well-in-the/m-p/640154#M25312</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-01-05T12:40:23Z</dc:date>
    </item>
  </channel>
</rss>