<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックPinMux Bug in LPCOpen?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PinMux-Bug-in-LPCOpen/m-p/638558#M25251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using pin P1.25 on an LPC1759 as a Match Register output pin. The documentation shows only 3 functions for that pin, with MAT1[1] as the third. However, I set it as IOCON_FUNC2 (third function), I get no output. I get expected output on that pin if I set it to IOCON_FUNC3 with the function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chip_IOCON_PinMuxSet(pIOCON, 1, 25, IOCON_MODE_INACT | IOCON_FUNC3);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance - james&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Oct 2016 00:59:25 GMT</pubDate>
    <dc:creator>jamesm</dc:creator>
    <dc:date>2016-10-15T00:59:25Z</dc:date>
    <item>
      <title>PinMux Bug in LPCOpen?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PinMux-Bug-in-LPCOpen/m-p/638558#M25251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using pin P1.25 on an LPC1759 as a Match Register output pin. The documentation shows only 3 functions for that pin, with MAT1[1] as the third. However, I set it as IOCON_FUNC2 (third function), I get no output. I get expected output on that pin if I set it to IOCON_FUNC3 with the function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chip_IOCON_PinMuxSet(pIOCON, 1, 25, IOCON_MODE_INACT | IOCON_FUNC3);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance - james&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Oct 2016 00:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PinMux-Bug-in-LPCOpen/m-p/638558#M25251</guid>
      <dc:creator>jamesm</dc:creator>
      <dc:date>2016-10-15T00:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: PinMux Bug in LPCOpen?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PinMux-Bug-in-LPCOpen/m-p/638559#M25252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="289017" data-username="jamesm" href="https://community.nxp.com/people/jamesm"&gt;James Massey&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;According to the reference manual, the P1.25 work as the MAT1.1 when select the Function 3 instead of the Function 2, as the fig 1 illustrate.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3873i90C7B801F2404197/image-size/large?v=v2&amp;amp;px=999" title="2016-10-18_13-58-08.jpg" alt="2016-10-18_13-58-08.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 06:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PinMux-Bug-in-LPCOpen/m-p/638559#M25252</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-10-18T06:02:20Z</dc:date>
    </item>
  </channel>
</rss>