<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC5410x FIFO in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-FIFO/m-p/638005#M25235</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it correct that the max FIFO size in the System FIFO for a UART is 16 bytes?&lt;/P&gt;&lt;P&gt;If this is so, I don't get why the system FIFO thing exists, why not just put the buffer in the UART like everyone else, or am I missing something?&lt;BR /&gt;Roger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Nov 2016 12:19:37 GMT</pubDate>
    <dc:creator>rogerlittlewood</dc:creator>
    <dc:date>2016-11-30T12:19:37Z</dc:date>
    <item>
      <title>LPC5410x FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-FIFO/m-p/638005#M25235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it correct that the max FIFO size in the System FIFO for a UART is 16 bytes?&lt;/P&gt;&lt;P&gt;If this is so, I don't get why the system FIFO thing exists, why not just put the buffer in the UART like everyone else, or am I missing something?&lt;BR /&gt;Roger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 12:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-FIFO/m-p/638005#M25235</guid>
      <dc:creator>rogerlittlewood</dc:creator>
      <dc:date>2016-11-30T12:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5410x FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-FIFO/m-p/638006#M25236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roger,&lt;/P&gt;&lt;P&gt;Yes, you're right.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 07:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-FIFO/m-p/638006#M25236</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-06T07:13:37Z</dc:date>
    </item>
  </channel>
</rss>