<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC54102 - DMA on 3 channels interrupts only one time instead of 3 times!</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-DMA-on-3-channels-interrupts-only-one-time-instead-of-3/m-p/637388#M25196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="287559" data-username="doini" href="https://community.nxp.com/people/doini"&gt;Doinita Marcu,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I was wondering if you upload the demo, then I can run the demo on the LPCXpresso54102 board to replicate the issue.&lt;/P&gt;&lt;P&gt;It will help me to figure out the cause of this issue&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Sep 2016 08:12:28 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-09-28T08:12:28Z</dc:date>
    <item>
      <title>LPC54102 - DMA on 3 channels interrupts only one time instead of 3 times!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-DMA-on-3-channels-interrupts-only-one-time-instead-of-3/m-p/637387#M25195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using 3 DMA channels triggered&amp;nbsp;at different times, shortly one after another, in an&amp;nbsp;interval of&amp;nbsp;several hundred of nano-seconds (the system frequency is 96MHz).&lt;/P&gt;&lt;P&gt;They are supposed to interrupt one after another at those&amp;nbsp;&lt;SPAN&gt;different times, but they interrupt only one time for the 3 channels.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Besides this, I am using linked DMA transfer, and it does not work. I am supposed to clear the interrupts after each descriptor was exhausted, but the 3 channels do not interrupt separately.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I mention that I set the transfer to reload each time the&amp;nbsp;descriptor was exhausted, but DMA does not reload, it will do only the first transfer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried to reload the next descriptors (into XFERCFG) manually inside the DMA interrupt, but the DMA transfer is not done completely.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would really appreciate any help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Doini&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 06:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-DMA-on-3-channels-interrupts-only-one-time-instead-of-3/m-p/637387#M25195</guid>
      <dc:creator>doini</dc:creator>
      <dc:date>2016-09-21T06:20:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 - DMA on 3 channels interrupts only one time instead of 3 times!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-DMA-on-3-channels-interrupts-only-one-time-instead-of-3/m-p/637388#M25196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="287559" data-username="doini" href="https://community.nxp.com/people/doini"&gt;Doinita Marcu,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I was wondering if you upload the demo, then I can run the demo on the LPCXpresso54102 board to replicate the issue.&lt;/P&gt;&lt;P&gt;It will help me to figure out the cause of this issue&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 08:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-DMA-on-3-channels-interrupts-only-one-time-instead-of-3/m-p/637388#M25196</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-28T08:12:28Z</dc:date>
    </item>
  </channel>
</rss>