<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ISO7816 on LPC11u68 in 115200 baudrate in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637096#M25183</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a standard java-card(2.2.2) &amp;nbsp;which actually is asynchronous smart card.Based on your code after running below code:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;CardClockOn(); /* Start clock at Ta */&lt;/P&gt;&lt;P&gt;//-----------------------------definition of&amp;nbsp;&lt;SPAN style="background-color: #f6f6f6;"&gt;CardClockOn function----&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;static __INLINE void CardClockOn(void)&lt;BR /&gt;{&lt;BR /&gt;// SC_PWM-&amp;gt;TCR = _BV(0);&lt;BR /&gt; LPC_IOCON-&amp;gt;PIO0_17 |= 0x03; /* UART SCLK */&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;As you can see inside body of &lt;SPAN style="background-color: #f6f6f6;"&gt;CardClockOn()&lt;/SPAN&gt;,only usart_clock function assign to the p0.17 and that's all,&lt;/P&gt;&lt;P&gt;Then how this cause clock generation on the p0.17 pin ? I also checked this pin with logic analyzer and there not any lock frequency on this pin.&lt;/P&gt;&lt;P&gt;-----------------&lt;/P&gt;&lt;P&gt;Also user manual explicitly said :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Synchronous mode should not be used with smart card mode.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Then how we can use USART0_Clock pin for providing clock to the card?&lt;/P&gt;&lt;P&gt;---------&lt;/P&gt;&lt;P&gt;Also from&amp;nbsp;&lt;STRONG&gt;11.7.8 Smart card mode&lt;/STRONG&gt;(user manual)&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The USART0 SCLK pin will output&lt;BR /&gt;synchronously with the data and at the data bit rate and may not be adequate for most&lt;BR /&gt;asynchronous cards.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;With best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Feb 2017 13:26:37 GMT</pubDate>
    <dc:creator>mahmoudhosseini</dc:creator>
    <dc:date>2017-02-04T13:26:37Z</dc:date>
    <item>
      <title>ISO7816 on LPC11u68 in 115200 baudrate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637093#M25180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every one,&lt;/P&gt;&lt;P&gt;we want to try lpc11u68 for contacting with a ISO7816 based smart Card.&lt;/P&gt;&lt;P&gt;As you know&amp;nbsp;this required using usart0 peripheral in iso7816 mode,Also clock pulses(CLK pins) must be generated separately(maybe using (SCTimer/PWM).&lt;/P&gt;&lt;P&gt;Does any one know whats maximum frequency &lt;SPAN&gt;SCTimer&amp;nbsp;&lt;/SPAN&gt;can generate?&lt;/P&gt;&lt;P&gt;I think for transitiving &amp;nbsp;in 115200 baud-rate we need 42.96 MHZ of clock frequency, Can SCTimer toggle a pin with this frequency?&lt;/P&gt;&lt;P&gt;As a other way Can we set Fi &amp;amp; Di parameters of ATR in any bigger value than 372 for transferring more data in the same clock frequency?&lt;/P&gt;&lt;P&gt;WBR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 07:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637093#M25180</guid>
      <dc:creator>mahmoudhosseini</dc:creator>
      <dc:date>2017-01-23T07:35:21Z</dc:date>
    </item>
    <item>
      <title>Re: ISO7816 on LPC11u68 in 115200 baudrate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637094#M25181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mahmoud,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could use as reference the smartcard example that comes with the following software package:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.lpcware.com/system/files/LPC11Uxx%20LPCXpresso%20Examples.zip" title="https://www.lpcware.com/system/files/LPC11Uxx%20LPCXpresso%20Examples.zip"&gt;https://www.lpcware.com/system/files/LPC11Uxx%20LPCXpresso%20Examples.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does your smart card allows the SCLK to be synchronously with the data and at the data bit rate? If yes you could better use the USART SCLK pin output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Smart card mode, OSInt is extended by FDINT. This extends the possible oversampling to 2048, as required to support ISO 7816-3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 22:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637094#M25181</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-01-27T22:38:48Z</dc:date>
    </item>
    <item>
      <title>Re: ISO7816 on LPC11u68 in 115200 baudrate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637095#M25182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for excellent answer,but how non-exact clock frequency does not affect to successful transition ?As I know new smart cards only use this clock pulses for synchronizing .Then I think any differences in clock frequency will cause a different ETU,which itself will cause mistake in receiving correct data. AM I true ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 09:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637095#M25182</guid>
      <dc:creator>mahmoudhosseini</dc:creator>
      <dc:date>2017-01-29T09:26:54Z</dc:date>
    </item>
    <item>
      <title>Re: ISO7816 on LPC11u68 in 115200 baudrate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637096#M25183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a standard java-card(2.2.2) &amp;nbsp;which actually is asynchronous smart card.Based on your code after running below code:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;CardClockOn(); /* Start clock at Ta */&lt;/P&gt;&lt;P&gt;//-----------------------------definition of&amp;nbsp;&lt;SPAN style="background-color: #f6f6f6;"&gt;CardClockOn function----&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;static __INLINE void CardClockOn(void)&lt;BR /&gt;{&lt;BR /&gt;// SC_PWM-&amp;gt;TCR = _BV(0);&lt;BR /&gt; LPC_IOCON-&amp;gt;PIO0_17 |= 0x03; /* UART SCLK */&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;As you can see inside body of &lt;SPAN style="background-color: #f6f6f6;"&gt;CardClockOn()&lt;/SPAN&gt;,only usart_clock function assign to the p0.17 and that's all,&lt;/P&gt;&lt;P&gt;Then how this cause clock generation on the p0.17 pin ? I also checked this pin with logic analyzer and there not any lock frequency on this pin.&lt;/P&gt;&lt;P&gt;-----------------&lt;/P&gt;&lt;P&gt;Also user manual explicitly said :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Synchronous mode should not be used with smart card mode.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Then how we can use USART0_Clock pin for providing clock to the card?&lt;/P&gt;&lt;P&gt;---------&lt;/P&gt;&lt;P&gt;Also from&amp;nbsp;&lt;STRONG&gt;11.7.8 Smart card mode&lt;/STRONG&gt;(user manual)&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The USART0 SCLK pin will output&lt;BR /&gt;synchronously with the data and at the data bit rate and may not be adequate for most&lt;BR /&gt;asynchronous cards.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;With best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 13:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/637096#M25183</guid>
      <dc:creator>mahmoudhosseini</dc:creator>
      <dc:date>2017-02-04T13:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: ISO7816 on LPC11u68 in 115200 baudrate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/1609803#M51809</link>
      <description>smartcard example link is broken.&lt;BR /&gt;pls, another link?</description>
      <pubDate>Mon, 06 Mar 2023 07:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISO7816-on-LPC11u68-in-115200-baudrate/m-p/1609803#M51809</guid>
      <dc:creator>wowfoot</dc:creator>
      <dc:date>2023-03-06T07:26:23Z</dc:date>
    </item>
  </channel>
</rss>