<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4088 USB-OTG External Transceiver required? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635560#M25093</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/soledad"&gt;soledad&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;If I want to use the same USB port as a device &amp;amp; as a host when connected to PC or when pendrive is connected to board respectively, do I necessarily need to use USB transceiver for this purpose?&lt;/P&gt;&lt;P&gt;I will not switch host &amp;amp; device without detaching the the USB(device/host). So if I put my board in device mode(default configuration) &amp;amp; when another device is attached ID level will trigger interrupt &amp;amp; then I will initialize board as host by removing pull up, adding pull downs, &amp;amp; applying VBUS(using switches &amp;amp; charge pump). Again when device is detached I will reinitialize it to device by removing pull downs, VBUS, &amp;amp; adding pull up. Will this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Priyank.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jan 2019 11:21:03 GMT</pubDate>
    <dc:creator>priyankb</dc:creator>
    <dc:date>2019-01-07T11:21:03Z</dc:date>
    <item>
      <title>LPC4088 USB-OTG External Transceiver required?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635558#M25091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I want to implement USB OTG on LPC4088. In user manual for OTG functionality external OTG transceiver(ISP1302) is used. LPC4088&amp;nbsp;has OTG controller.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is it necessary to use external transceiver for OTG functionality?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 04:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635558#M25091</guid>
      <dc:creator>amitkolekar</dc:creator>
      <dc:date>2017-03-09T04:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 USB-OTG External Transceiver required?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635559#M25092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, for full OTG compliant it is necessary to add externally the OTG transceiver (ISP1302). This is in order to manage the pins Vbus &amp;amp; ID in addition to control "on the fly" the Host or Device stack.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 22:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635559#M25092</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-04-04T22:01:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 USB-OTG External Transceiver required?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635560#M25093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/soledad"&gt;soledad&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;If I want to use the same USB port as a device &amp;amp; as a host when connected to PC or when pendrive is connected to board respectively, do I necessarily need to use USB transceiver for this purpose?&lt;/P&gt;&lt;P&gt;I will not switch host &amp;amp; device without detaching the the USB(device/host). So if I put my board in device mode(default configuration) &amp;amp; when another device is attached ID level will trigger interrupt &amp;amp; then I will initialize board as host by removing pull up, adding pull downs, &amp;amp; applying VBUS(using switches &amp;amp; charge pump). Again when device is detached I will reinitialize it to device by removing pull downs, VBUS, &amp;amp; adding pull up. Will this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Priyank.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 11:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-USB-OTG-External-Transceiver-required/m-p/635560#M25093</guid>
      <dc:creator>priyankb</dc:creator>
      <dc:date>2019-01-07T11:21:03Z</dc:date>
    </item>
  </channel>
</rss>