<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programming an NXP - LPC1313FBD48 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-an-NXP-LPC1313FBD48/m-p/634006#M24980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;According to your statement, I'd like to suggest that two approach to program the LPC devices.&lt;/P&gt;&lt;P&gt;1. Using the debugger, such as J-link, U-link, etc. and the debug interface supports the SWD and JTAG.&lt;/P&gt;&lt;P&gt;2. Using the ISP mode to program the MCU, you can choose the UART TTL Serial cable to connect the MCU to the PC and you should go to the &lt;A class="link-titled" href="http://www.flashmagictool.com/" title="http://www.flashmagictool.com/"&gt;Flash Magic - Welcome&lt;/A&gt;&amp;nbsp; follow the instructions of the Flash Magic tool.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Dec 2016 01:53:47 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-12-27T01:53:47Z</dc:date>
    <item>
      <title>Programming an NXP - LPC1313FBD48</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-an-NXP-LPC1313FBD48/m-p/634005#M24979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;IMG alt="" class="image-1 jive-image j-img-original" src="http://www.kynix.com/images/ic-package/QFP.jpg" style="height: auto;" /&gt;&lt;/P&gt;&lt;P&gt;I was planning on flashing my mini os onto my NXP - LPC1313FBD48 (&lt;A href="http://www.kynix.com/Detail/25017/LPC1313FBD48.html"&gt;here&lt;/A&gt; is a link to where I bought it) but I wasn't really sure how. So I asked but I was told that I would need a serial to usb connector. I wasn't sure if they meant something like This or something like this. So my questions are&lt;/P&gt;&lt;P&gt;Which connector do I use and how do I pick the connector?&lt;BR /&gt;How do I use the connector with my MCU (ex. Plug one end into my usb connector and put Jumper wires onto certain ports of my MCU inorder to send the data)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 08:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-an-NXP-LPC1313FBD48/m-p/634005#M24979</guid>
      <dc:creator>ffff</dc:creator>
      <dc:date>2016-12-22T08:37:33Z</dc:date>
    </item>
    <item>
      <title>Re: Programming an NXP - LPC1313FBD48</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-an-NXP-LPC1313FBD48/m-p/634006#M24980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;According to your statement, I'd like to suggest that two approach to program the LPC devices.&lt;/P&gt;&lt;P&gt;1. Using the debugger, such as J-link, U-link, etc. and the debug interface supports the SWD and JTAG.&lt;/P&gt;&lt;P&gt;2. Using the ISP mode to program the MCU, you can choose the UART TTL Serial cable to connect the MCU to the PC and you should go to the &lt;A class="link-titled" href="http://www.flashmagictool.com/" title="http://www.flashmagictool.com/"&gt;Flash Magic - Welcome&lt;/A&gt;&amp;nbsp; follow the instructions of the Flash Magic tool.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 01:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-an-NXP-LPC1313FBD48/m-p/634006#M24980</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-27T01:53:47Z</dc:date>
    </item>
  </channel>
</rss>