<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPCXpresso54608</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608/m-p/630554#M24804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;For some time now I have been looking for an opportunity to implement a 220 V Solar Microinverter&amp;nbsp; (36 V PV module) around an LPC processor.&lt;/SPAN&gt; &lt;SPAN class=""&gt;I believe the LPCXpresso54608 board has the necessary features.&lt;/SPAN&gt; &lt;SPAN class=""&gt;In addition to the inherent low power consumption, the Cortex-M4 180 MHz microcontroller performance (with DSP, 64 bit MAC, SIMD, saturation, etc.) becomes the brain controlling power flow from the PV panel to the grid.&amp;nbsp; Also, the LPC54608 would be responsible to execute the MPPT algorithm, fault control, and Ethernet communication (ie. hosting a simple web page for configuration and monitoring). My initial specifications: Maximum output power: 190 W, Nominal output voltage: 220 V, Power factor: Greater than 0.95, Total harmonic distortion: Less than 5%. The SCT outputs are particularly useful in order to generate de PWM signals, The SCT inputs can provide&amp;nbsp; fault alarms for shutdown the converter. The support for graphical LCD allows building an HMI for local user control.The attached figure illustrates the basic configuration, where the topology for the converter can vary for example, for an interleaved flayback. After the proof of concept and the validation tests I would like to change this design to a "Grid-Connected Solar Micro Inverter".&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Dec 2016 17:47:03 GMT</pubDate>
    <dc:creator>dirceurodrigues</dc:creator>
    <dc:date>2016-12-20T17:47:03Z</dc:date>
    <item>
      <title>LPCXpresso54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608/m-p/630554#M24804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;For some time now I have been looking for an opportunity to implement a 220 V Solar Microinverter&amp;nbsp; (36 V PV module) around an LPC processor.&lt;/SPAN&gt; &lt;SPAN class=""&gt;I believe the LPCXpresso54608 board has the necessary features.&lt;/SPAN&gt; &lt;SPAN class=""&gt;In addition to the inherent low power consumption, the Cortex-M4 180 MHz microcontroller performance (with DSP, 64 bit MAC, SIMD, saturation, etc.) becomes the brain controlling power flow from the PV panel to the grid.&amp;nbsp; Also, the LPC54608 would be responsible to execute the MPPT algorithm, fault control, and Ethernet communication (ie. hosting a simple web page for configuration and monitoring). My initial specifications: Maximum output power: 190 W, Nominal output voltage: 220 V, Power factor: Greater than 0.95, Total harmonic distortion: Less than 5%. The SCT outputs are particularly useful in order to generate de PWM signals, The SCT inputs can provide&amp;nbsp; fault alarms for shutdown the converter. The support for graphical LCD allows building an HMI for local user control.The attached figure illustrates the basic configuration, where the topology for the converter can vary for example, for an interleaved flayback. After the proof of concept and the validation tests I would like to change this design to a "Grid-Connected Solar Micro Inverter".&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 17:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608/m-p/630554#M24804</guid>
      <dc:creator>dirceurodrigues</dc:creator>
      <dc:date>2016-12-20T17:47:03Z</dc:date>
    </item>
  </channel>
</rss>