<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: DAC / ADC sharing</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629777#M24763</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, the use of the DAC blocks channel 0 of both ADC0 and ADC1. The reason is that the ADC0_0/ADC1_0/DAC pin hardwires them all together.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Nov 2016 23:59:35 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2016-11-04T23:59:35Z</dc:date>
    <item>
      <title>DAC / ADC sharing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629776#M24762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if I am reading the users manual correctly for the LPC1837...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning sharing DAC and ADC0, if I am using the DAC on pin B2, is the ADC0_0 unavailable on package position C2. &amp;nbsp;I am using the LBGA256 package. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 16:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629776#M24762</guid>
      <dc:creator>tonyvink</dc:creator>
      <dc:date>2016-11-03T16:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: DAC / ADC sharing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629777#M24763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, the use of the DAC blocks channel 0 of both ADC0 and ADC1. The reason is that the ADC0_0/ADC1_0/DAC pin hardwires them all together.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2016 23:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629777#M24763</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-11-04T23:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: DAC / ADC sharing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629778#M24764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Carlos.&lt;/P&gt;&lt;P&gt;I would have replied sooner but I guess I was looking in the wrong place. &amp;nbsp;Thought I posted in the LPC1837 section but guess I messed something up when posting.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 21:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-ADC-sharing/m-p/629778#M24764</guid>
      <dc:creator>tonyvink</dc:creator>
      <dc:date>2016-11-07T21:52:44Z</dc:date>
    </item>
  </channel>
</rss>