<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCxpresso1769 (OM13085) configure SWO? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso1769-OM13085-configure-SWO/m-p/629542#M24759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that the LPCXpresso1769/CD board's built in debug probe does not support SWO tracing - you need an LPC-Link2 to carry this out. For more details, please see&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389084"&gt;https://community.nxp.com/thread/389084&lt;/A&gt;&amp;nbsp; along with the the trace guide supplied inside the LPCXpresso installation directory / built in help system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 17:14:53 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-10-12T17:14:53Z</dc:date>
    <item>
      <title>LPCxpresso1769 (OM13085) configure SWO?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso1769-OM13085-configure-SWO/m-p/629541#M24758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have OM13085 board and&amp;nbsp;LPCXpresso v8.2.2 on Win10. &amp;nbsp; &amp;nbsp;I can build the example projects and load/debug code but the SWO features don't seem to work. &amp;nbsp; The SWO Trace Configuration shows green lights for SWD connection, clock speed, probe backend, &amp;nbsp;probe, baud. &amp;nbsp; &amp;nbsp;The "probe configured" and "target configured" &amp;nbsp;indicators are NOT green. &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3549iE1A54E712147569F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I can load code and debug/single step but would like to use the SWO Trace features. &amp;nbsp; &amp;nbsp;What can I do to get the SWO trace configured properly?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 15:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso1769-OM13085-configure-SWO/m-p/629541#M24758</guid>
      <dc:creator>jameslittlefiel</dc:creator>
      <dc:date>2016-10-12T15:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso1769 (OM13085) configure SWO?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso1769-OM13085-configure-SWO/m-p/629542#M24759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that the LPCXpresso1769/CD board's built in debug probe does not support SWO tracing - you need an LPC-Link2 to carry this out. For more details, please see&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389084"&gt;https://community.nxp.com/thread/389084&lt;/A&gt;&amp;nbsp; along with the the trace guide supplied inside the LPCXpresso installation directory / built in help system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 17:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso1769-OM13085-configure-SWO/m-p/629542#M24759</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-10-12T17:14:53Z</dc:date>
    </item>
  </channel>
</rss>