<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: value of pull down resistor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628090#M24694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi KS,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's the &lt;EM&gt;&lt;STRONG&gt;weak&lt;/STRONG&gt;&lt;/EM&gt; pull-up and pull-down what is meant by the terms pull-up and pull-down resistor&amp;nbsp;throughout the user manual and data sheet.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;strong&lt;/STRONG&gt;&lt;/EM&gt; pull-up and pull-down in the block diagram you've posted represent the push-pull output stage of the pin! They are never referred to as pull-up or pull-down anywhere else in user manual or data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Technically both are MOSFET's with a certain ON resistance when enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The (weak) pull-up and pull-down MOSFET's are equivalent (typically) to a resistor of 60k. The data sheet &amp;nbsp; contains an incorrect non-linear V-I characteristic of the pull-up and pull-down (figures 19/20 in data sheet 2.2). This non-linear behaviour applies to older chip generations (e.g. early LPC1114) only. On LPC11U37 both pull-up and pull-down are almost perfectly linear resistors over the whole input voltage range (0...VDD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the push-pull output stage (the strong version), the MOSFET's also act like linear resistors of typically 50 Ohms (max 100 Ohms) while in their operating area (which we specify up to 4 mA current). They are short-circuit protected, so they will saturate when output current becomes to high.&lt;/P&gt;&lt;P&gt;See figures 17/18 for the typical values, table 5 for the worst case values. Note that the high-side driver of the PIO0_7 output stage is different as it can drive several times the current of a standard port pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Sep 2016 10:29:16 GMT</pubDate>
    <dc:creator>rolfmeeser</dc:creator>
    <dc:date>2016-09-19T10:29:16Z</dc:date>
    <item>
      <title>value of pull down resistor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628089#M24693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi supporters,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;customer is designing LPC11U37 and needs to know below four numbers(strong pull-up、strong pull-down、weak pull-up and weak pull-down) which datasheet doesn't explain it, please help to provide this thanks.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5219iAEB3901DCE536E55/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 03:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628089#M24693</guid>
      <dc:creator>K_S_Lin</dc:creator>
      <dc:date>2016-09-19T03:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: value of pull down resistor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628090#M24694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi KS,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's the &lt;EM&gt;&lt;STRONG&gt;weak&lt;/STRONG&gt;&lt;/EM&gt; pull-up and pull-down what is meant by the terms pull-up and pull-down resistor&amp;nbsp;throughout the user manual and data sheet.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;strong&lt;/STRONG&gt;&lt;/EM&gt; pull-up and pull-down in the block diagram you've posted represent the push-pull output stage of the pin! They are never referred to as pull-up or pull-down anywhere else in user manual or data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Technically both are MOSFET's with a certain ON resistance when enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The (weak) pull-up and pull-down MOSFET's are equivalent (typically) to a resistor of 60k. The data sheet &amp;nbsp; contains an incorrect non-linear V-I characteristic of the pull-up and pull-down (figures 19/20 in data sheet 2.2). This non-linear behaviour applies to older chip generations (e.g. early LPC1114) only. On LPC11U37 both pull-up and pull-down are almost perfectly linear resistors over the whole input voltage range (0...VDD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the push-pull output stage (the strong version), the MOSFET's also act like linear resistors of typically 50 Ohms (max 100 Ohms) while in their operating area (which we specify up to 4 mA current). They are short-circuit protected, so they will saturate when output current becomes to high.&lt;/P&gt;&lt;P&gt;See figures 17/18 for the typical values, table 5 for the worst case values. Note that the high-side driver of the PIO0_7 output stage is different as it can drive several times the current of a standard port pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 10:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628090#M24694</guid>
      <dc:creator>rolfmeeser</dc:creator>
      <dc:date>2016-09-19T10:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: value of pull down resistor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628091#M24695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got it, thanks Rolf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 03:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/value-of-pull-down-resistor/m-p/628091#M24695</guid>
      <dc:creator>K_S_Lin</dc:creator>
      <dc:date>2016-10-04T03:32:49Z</dc:date>
    </item>
  </channel>
</rss>