<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1769 webserver</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-webserver/m-p/624535#M24521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on &amp;nbsp;MCB1700 Board &amp;nbsp;with webserver example . But After sometime of ping webserver is crash and &amp;nbsp;program got stuck in Hardfault Handler . If i analysed call stack window then it shows that hard fault handler is due to malloc. So what will be the cause of this?&lt;/P&gt;&lt;P&gt;lpc1769‌&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/webserver/tg-p"&gt;#webserver&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Mar 2017 09:49:53 GMT</pubDate>
    <dc:creator>djtilava</dc:creator>
    <dc:date>2017-03-28T09:49:53Z</dc:date>
    <item>
      <title>LPC1769 webserver</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-webserver/m-p/624535#M24521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on &amp;nbsp;MCB1700 Board &amp;nbsp;with webserver example . But After sometime of ping webserver is crash and &amp;nbsp;program got stuck in Hardfault Handler . If i analysed call stack window then it shows that hard fault handler is due to malloc. So what will be the cause of this?&lt;/P&gt;&lt;P&gt;lpc1769‌&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/webserver/tg-p"&gt;#webserver&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 09:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-webserver/m-p/624535#M24521</guid>
      <dc:creator>djtilava</dc:creator>
      <dc:date>2017-03-28T09:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 webserver</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-webserver/m-p/624536#M24522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Divyesh,&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We found a workaround to resolve this issue in the webserver project&amp;nbsp; on LPC1769 , the suggested workaround is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the tcp_impl.h file change the definition of TCP_MSL to the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#define TCP_MSL 100 //1000 //60000UL /* The maximum segment lifetime in milliseconds */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means the memory is freed more quickly when closing connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the value 100 and 1000 on lpcopen webserver example on lpc1788 and it can work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We analyze the cause should be that when TCP connection is closed, the PCB is not released in time due to the long (120s) time waiting. This cause the PCB created more and more so that memory leaks due to the limited memory of MCU (SRAM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 23:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-webserver/m-p/624536#M24522</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-03-29T23:20:59Z</dc:date>
    </item>
  </channel>
</rss>