<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1800 VBUS Pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622105#M24385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding of the remark is that writing/setting has no effect, not necessarily means reading.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because VBUS is an input signal, not like general I/O.&lt;/P&gt;&lt;P&gt;May be you can test and verify it with a board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Nov 2016 09:08:35 GMT</pubDate>
    <dc:creator>ericding</dc:creator>
    <dc:date>2016-11-25T09:08:35Z</dc:date>
    <item>
      <title>LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622100#M24380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer is using the LPC1800 for a USB application. Now they want to use the VBUS Pin of the USB1 Interface to discover Connect/Disconnect conditions. How is this done?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter . &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 14:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622100#M24380</guid>
      <dc:creator>peter_furtner</dc:creator>
      <dc:date>2016-11-24T14:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622101#M24381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain more of this application?&lt;/P&gt;&lt;P&gt;Is LPC1800 used as a USB host or device?&lt;/P&gt;&lt;P&gt;It's the device's responsibility to actively connect to the host, and host may need to provide power to the device via VBUS pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 03:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622101#M24381</guid>
      <dc:creator>ericding</dc:creator>
      <dc:date>2016-11-25T03:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622102#M24382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric, &lt;/P&gt;&lt;P&gt;the LPC1800 USB1 Interface is used as USB-Device.&lt;/P&gt;&lt;P&gt;The customer wants to discover the case that the USB gets disconneted from the host (i.e. the USB-Cable gets unplugged)&lt;/P&gt;&lt;P&gt;In this case the VBUS Signal on the pin gets LOW (because of the external Pull-Down). But the customer doesn't know, which bit in any of the internal Registers to read to discover this case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 07:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622102#M24382</guid>
      <dc:creator>peter_furtner</dc:creator>
      <dc:date>2016-11-25T07:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622103#M24383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below descriptions may give you some hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11284i001158E024E9493E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 08:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622103#M24383</guid>
      <dc:creator>ericding</dc:creator>
      <dc:date>2016-11-25T08:20:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622104#M24384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;the message also says “REMARK: The setting of this bit has no effect if the USB1_VBUS function of P2_5 is enabled through the SFSP2_5 register.“&lt;/P&gt;&lt;P&gt;The customer did enable the USB1_VBUS Signal through SFSP2_5. Otherwise he would not get the external signal into the device.&lt;/P&gt;&lt;P&gt;Still, the question is: How can he read the status of the external VBUS Signal in the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 08:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622104#M24384</guid>
      <dc:creator>peter_furtner</dc:creator>
      <dc:date>2016-11-25T08:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622105#M24385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding of the remark is that writing/setting has no effect, not necessarily means reading.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because VBUS is an input signal, not like general I/O.&lt;/P&gt;&lt;P&gt;May be you can test and verify it with a board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 09:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622105#M24385</guid>
      <dc:creator>ericding</dc:creator>
      <dc:date>2016-11-25T09:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622106#M24386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;BR /&gt;&lt;BR /&gt;P2_5 is an input to the USB1 full speed transceiver which works as a VBUS power detector. This sensing input is then automatically controlling the internal &lt;EM&gt;vbus_valid&lt;/EM&gt; signal.&lt;/P&gt;&lt;P&gt;In case you don't use this transceiver input at pin P2_5, you could use any other GPIO or an ADC input to sense the VBUS signal level. By means of polling or with a level triggered interrupt you can then write by software into the bit USB_VBUS and control the internal signal &lt;EM&gt;vbus_valid&lt;/EM&gt; by software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 13:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622106#M24386</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2016-11-30T13:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1800 VBUS Pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622107#M24387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernhard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your detailed clarification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 06:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1800-VBUS-Pin/m-p/622107#M24387</guid>
      <dc:creator>ericding</dc:creator>
      <dc:date>2016-12-01T06:22:31Z</dc:date>
    </item>
  </channel>
</rss>