<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Receive Data From BLE and Printing it on LPCXpresso's consol</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621942#M24375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would be helpful if you provided an actual description of what your problem actually is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are trying to have your application display the output from printf() calls to the debugger's console view, then for LPCOpen based applications you need to make sure that your board library is configured correctly. For more details see:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/390662"&gt;LPCOpen debug input/output support&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional&amp;nbsp;information on LPCXpresso IDE's printf() support can be found at:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/389140"&gt;Using printf()&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2016 09:38:49 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-12-19T09:38:49Z</dc:date>
    <item>
      <title>Receive Data From BLE and Printing it on LPCXpresso's consol</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621941#M24374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can some tell me what is wrong with code please?&lt;/P&gt;&lt;P&gt;I want to receive data from HC-06 BLE connected with UART1 LPC4330.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#if defined (__USE_LPCOPEN)&lt;BR /&gt;#if defined(NO_BOARD_LIB)&lt;BR /&gt;#include "chip.h"&lt;BR /&gt;#else&lt;BR /&gt;#include "board.h"&lt;BR /&gt;#endif&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#include &amp;lt;cr_section_macros.h&amp;gt;&lt;/P&gt;&lt;P&gt;// TODO: insert other include files here&lt;/P&gt;&lt;P&gt;// TODO: insert other definitions and declarations here&lt;BR /&gt;#define BOARD_NGX_XPLORER_4330&lt;BR /&gt;#define UARTNum 1&lt;BR /&gt;#define LPC_UART LPC_UART1&lt;BR /&gt;#define UARTx_IRQn UART1_IRQn&lt;BR /&gt;#define UARTx_IRQHandler UART1_IRQHandler&lt;BR /&gt;#define _GPDMA_CONN_UART_Tx GPDMA_CONN_UART1_Tx&lt;BR /&gt;#define _GPDMA_CONN_UART_Rx GPDMA_CONN_UART1_Rx&lt;/P&gt;&lt;P&gt;/* Transmit and receive ring buffers */&lt;BR /&gt;STATIC RINGBUFF_T txring, rxring;&lt;/P&gt;&lt;P&gt;/* Ring buffer size */&lt;BR /&gt;#define UART_RB_SIZE 256&lt;/P&gt;&lt;P&gt;/* Transmit and receive buffers */&lt;BR /&gt;static uint8_t rxbuff[UART_RB_SIZE], txbuff[UART_RB_SIZE];&lt;/P&gt;&lt;P&gt;static uint8_t uartABStart[] = "Starting UART Auto-Baud - Press 'A' or 'a'! \n\r";&lt;BR /&gt;static uint8_t uartABComplete[] = "UART Auto-Baudrate synchronized! \n\r";&lt;/P&gt;&lt;P&gt;/* Uart Polling variables and functions declaration */&lt;BR /&gt;static uint8_t uartPolling_menu1[] = "Hello NXP Semiconductors \r\n";&lt;BR /&gt;static uint8_t uartPolling_menu2[] = "UART polling mode demo \r\n";&lt;BR /&gt;static uint8_t uartPolling_menu3[] = "\r\nUART demo terminated!";&lt;BR /&gt;static uint8_t uartPolling_menu4[] = "\r\nPress number 1-3 to choose UART running mode:\r\n"&lt;BR /&gt; "\t 1: Polling Mode \r\n"&lt;BR /&gt; "\t 2: Interrupt Mode \r\n"&lt;BR /&gt; "\t 3: DMA Mode \r\n";&lt;BR /&gt;static uint8_t uartPolling_menu5[] = "\r\nPolling mode is running now! Please press \'c\' and choose another mode \r\n";&lt;/P&gt;&lt;P&gt;/* Uart Interrupt variables and functions declaration */&lt;BR /&gt;static uint8_t uart_interrupt_menu[] =&lt;BR /&gt; "UART Interrupt mode demo ! \r\nPress '1' to '4' to display 4 menus \r\nPress 'x'to exit UART interrupt mode \r\n";&lt;BR /&gt;static uint8_t uart_interrupt_menu1[] = "UART interrupt menu 1 \r\n";&lt;BR /&gt;static uint8_t uart_interrupt_menu2[] = "UART interrupt menu 2 \r\n";&lt;BR /&gt;static uint8_t uart_interrupt_menu3[] = "UART interrupt menu 3 \r\n";&lt;BR /&gt;static uint8_t uart_interrupt_menu4[] = "UART interrupt menu 4 \r\n";&lt;BR /&gt;/* static uint8_t rxUartIntBuf[1]; */&lt;/P&gt;&lt;P&gt;#define DMA_TIMEOUT 0xA000000&lt;BR /&gt;/* DMA variables and functions declaration */&lt;BR /&gt;static uint8_t dmaChannelNumTx, dmaChannelNumRx;&lt;BR /&gt;static uint8_t uartDMA_menu[] = "Hello NXP Semiconductors (DMA mode)\r\n"&lt;BR /&gt; "UART DMA mode demo ! Please type 'hello NXP' to return\r\n";&lt;/P&gt;&lt;P&gt;static volatile uint32_t channelTC; /* Terminal Counter flag for Channel */&lt;BR /&gt;static volatile uint32_t channelTCErr;&lt;BR /&gt;static FunctionalState isDMATx = ENABLE;&lt;/P&gt;&lt;P&gt;/*****************************************************************************&lt;BR /&gt; * Public types/enumerations/variables&lt;BR /&gt; ****************************************************************************/&lt;/P&gt;&lt;P&gt;/*****************************************************************************&lt;BR /&gt; * Private functions&lt;BR /&gt; ****************************************************************************/&lt;/P&gt;&lt;P&gt;/* Initialize DMA for UART, enable DMA controller and enable DMA interrupt */&lt;BR /&gt;static void App_DMA_Init(void)&lt;BR /&gt;{&lt;BR /&gt; /* Initialize GPDMA controller */&lt;BR /&gt; Chip_GPDMA_Init(LPC_GPDMA);&lt;BR /&gt; /* Setting GPDMA interrupt */&lt;BR /&gt; NVIC_DisableIRQ(DMA_IRQn);&lt;BR /&gt; NVIC_SetPriority(DMA_IRQn, ((0x01 &amp;lt;&amp;lt; 3) | 0x01));&lt;BR /&gt; NVIC_EnableIRQ(DMA_IRQn);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* DeInitialize DMA for UART, free transfer channels and disable DMA interrupt */&lt;BR /&gt;static void App_DMA_DeInit(void)&lt;BR /&gt;{&lt;BR /&gt; Chip_GPDMA_Stop(LPC_GPDMA, dmaChannelNumTx);&lt;BR /&gt; Chip_GPDMA_Stop(LPC_GPDMA, dmaChannelNumRx);&lt;BR /&gt; NVIC_DisableIRQ(DMA_IRQn);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* DMA routine for example_uart */&lt;BR /&gt;static void App_DMA_Test(void)&lt;BR /&gt;{&lt;BR /&gt; uint8_t receiveBuffer[16];&lt;/P&gt;&lt;P&gt;App_DMA_Init();&lt;BR /&gt; dmaChannelNumTx = Chip_GPDMA_GetFreeChannel(LPC_GPDMA, _GPDMA_CONN_UART_Tx);&lt;/P&gt;&lt;P&gt;isDMATx = ENABLE;&lt;BR /&gt; channelTC = channelTCErr = 0;&lt;BR /&gt; Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumTx,&lt;BR /&gt; (uint32_t) &amp;amp;uartDMA_menu[0],&lt;BR /&gt; _GPDMA_CONN_UART_Tx,&lt;BR /&gt; GPDMA_TRANSFERTYPE_M2P_CONTROLLER_DMA,&lt;BR /&gt; sizeof(uartDMA_menu));&lt;BR /&gt; while (!channelTC) {}&lt;/P&gt;&lt;P&gt;dmaChannelNumRx = Chip_GPDMA_GetFreeChannel(LPC_GPDMA, _GPDMA_CONN_UART_Rx);&lt;BR /&gt; isDMATx = DISABLE;&lt;BR /&gt; channelTC = channelTCErr = 0;&lt;BR /&gt; Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumRx,&lt;BR /&gt; _GPDMA_CONN_UART_Rx,&lt;BR /&gt; (uint32_t) &amp;amp;receiveBuffer[0],&lt;BR /&gt; GPDMA_TRANSFERTYPE_P2M_CONTROLLER_DMA,&lt;BR /&gt; 10);&lt;BR /&gt; while (!channelTC) {}&lt;/P&gt;&lt;P&gt;isDMATx = ENABLE;&lt;BR /&gt; channelTC = channelTCErr = 0;&lt;BR /&gt; Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumTx,&lt;BR /&gt; (uint32_t) &amp;amp;receiveBuffer[0],&lt;BR /&gt; _GPDMA_CONN_UART_Tx,&lt;BR /&gt; GPDMA_TRANSFERTYPE_M2P_CONTROLLER_DMA,&lt;BR /&gt; 10);&lt;BR /&gt; while (!channelTC) {}&lt;/P&gt;&lt;P&gt;App_DMA_DeInit();&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Print Welcome Screen Menu subroutine by Interrupt mode */&lt;BR /&gt;static void Print_Menu_Interrupt(LPC_USART_T *UARTx)&lt;BR /&gt;{&lt;BR /&gt; uint32_t tmp;&lt;BR /&gt; uint8_t *pDat;&lt;/P&gt;&lt;P&gt;tmp = sizeof(uart_interrupt_menu);&lt;BR /&gt; pDat = (uint8_t *) &amp;amp;uart_interrupt_menu[0];&lt;BR /&gt; Chip_UART_SendRB(UARTx, &amp;amp;txring, pDat, tmp);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Initialize Interrupt for UART */&lt;BR /&gt;static void App_Interrupt_Init(void)&lt;BR /&gt;{&lt;BR /&gt; /* Enable UART Rx &amp;amp; line status interrupts */&lt;BR /&gt; /*&lt;BR /&gt; * Do not enable transmit interrupt here, since it is handled by&lt;BR /&gt; * UART_Send() function, just to reset Tx Interrupt state for the&lt;BR /&gt; * first time&lt;BR /&gt; */&lt;BR /&gt; Chip_UART_IntEnable(LPC_UART, (UART_IER_RBRINT | UART_IER_RLSINT));&lt;/P&gt;&lt;P&gt;/* Before using the ring buffers, initialize them using the ring&lt;BR /&gt; buffer init function */&lt;BR /&gt; RingBuffer_Init(&amp;amp;rxring, rxbuff, 1, UART_RB_SIZE);&lt;BR /&gt; RingBuffer_Init(&amp;amp;txring, txbuff, 1, UART_RB_SIZE);&lt;/P&gt;&lt;P&gt;/* Enable Interrupt for UART channel */&lt;BR /&gt; /* Priority = 1 */&lt;BR /&gt; NVIC_SetPriority(UARTx_IRQn, 1);&lt;BR /&gt; /* Enable Interrupt for UART channel */&lt;BR /&gt; NVIC_EnableIRQ(UARTx_IRQn);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* DeInitialize Interrupt for UART */&lt;BR /&gt;static void App_Interrupt_DeInit(void)&lt;BR /&gt;{&lt;BR /&gt; /* Disable UART Rx &amp;amp; line status interrupts */&lt;BR /&gt; Chip_UART_IntDisable(LPC_UART, (UART_IER_RBRINT | UART_IER_RLSINT));&lt;/P&gt;&lt;P&gt;/* Disable Interrupt for UART channel */&lt;BR /&gt; NVIC_DisableIRQ(UARTx_IRQn);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Interrupt routine for example_uart */&lt;BR /&gt;static void App_Interrupt_Test(void)&lt;BR /&gt;{&lt;BR /&gt; uint8_t isExit = 0, userInput;&lt;BR /&gt; int len;&lt;BR /&gt; App_Interrupt_Init();&lt;/P&gt;&lt;P&gt;/* Print out uart interrupt menu */&lt;BR /&gt; Print_Menu_Interrupt(LPC_UART);&lt;/P&gt;&lt;P&gt;while (!isExit) {&lt;BR /&gt; len = 0;&lt;BR /&gt; while (len == 0) {&lt;BR /&gt; len = Chip_UART_ReadRB(LPC_UART, &amp;amp;rxring, &amp;amp;userInput, 1);&lt;BR /&gt; }&lt;BR /&gt; if (userInput == '1') {&lt;BR /&gt; Chip_UART_SendRB(LPC_UART, &amp;amp;txring, (uint8_t *) &amp;amp;uart_interrupt_menu1[0], sizeof(uart_interrupt_menu1));&lt;BR /&gt; }&lt;BR /&gt; else if (userInput == '2') {&lt;BR /&gt; Chip_UART_SendRB(LPC_UART, &amp;amp;txring, (uint8_t *) &amp;amp;uart_interrupt_menu2[0], sizeof(uart_interrupt_menu2));&lt;BR /&gt; }&lt;BR /&gt; else if (userInput == '3') {&lt;BR /&gt; Chip_UART_SendRB(LPC_UART, &amp;amp;txring, (uint8_t *) &amp;amp;uart_interrupt_menu3[0], sizeof(uart_interrupt_menu3));&lt;BR /&gt; }&lt;BR /&gt; else if (userInput == '4') {&lt;BR /&gt; Chip_UART_SendRB(LPC_UART, &amp;amp;txring, (uint8_t *) &amp;amp;uart_interrupt_menu4[0], sizeof(uart_interrupt_menu4));&lt;BR /&gt; }&lt;BR /&gt; else if (( userInput == 'x') || ( userInput == 'X') ) {&lt;BR /&gt; isExit = 1;&lt;BR /&gt; }&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;App_Interrupt_DeInit();&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Print Welcome menu by Polling mode */&lt;BR /&gt;static void Print_Menu_Polling(void)&lt;BR /&gt;{&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu1, sizeof(uartPolling_menu1));&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu2, sizeof(uartPolling_menu2));&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu5, sizeof(uartPolling_menu5));&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/*****************************************************************************&lt;BR /&gt; * Public functions&lt;BR /&gt; ****************************************************************************/&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief GPDMA interrupt handler sub-routine&lt;BR /&gt; * @return Nothing&lt;BR /&gt; */&lt;BR /&gt;void DMA_IRQHandler(void)&lt;BR /&gt;{&lt;BR /&gt; uint8_t dmaChannelNum;&lt;BR /&gt; if (isDMATx) {&lt;BR /&gt; dmaChannelNum = dmaChannelNumTx;&lt;BR /&gt; }&lt;BR /&gt; else {&lt;BR /&gt; dmaChannelNum = dmaChannelNumRx;&lt;BR /&gt; }&lt;BR /&gt; if (Chip_GPDMA_Interrupt(LPC_GPDMA, dmaChannelNum) == SUCCESS) {&lt;BR /&gt; channelTC++;&lt;BR /&gt; }&lt;BR /&gt; else {&lt;BR /&gt; channelTCErr++;&lt;BR /&gt; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief UART interrupt handler sub-routine&lt;BR /&gt; * @return Nothing&lt;BR /&gt; */&lt;BR /&gt;void UARTx_IRQHandler(void)&lt;BR /&gt;{&lt;BR /&gt; Chip_UART_IRQRBHandler(LPC_UART, &amp;amp;rxring, &amp;amp;txring);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief Main UART program body&lt;BR /&gt; * @return Always returns -1&lt;BR /&gt; */&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int main(void) {&lt;/P&gt;&lt;P&gt;#if defined (__USE_LPCOPEN)&lt;BR /&gt; // Read clock settings and update SystemCoreClock variable&lt;BR /&gt; SystemCoreClockUpdate();&lt;BR /&gt;#if !defined(NO_BOARD_LIB)&lt;BR /&gt;#if defined (__MULTICORE_MASTER) || defined (__MULTICORE_NONE)&lt;BR /&gt; // Set up and initialize all required blocks and&lt;BR /&gt; // functions related to the board hardware&lt;BR /&gt; Board_Init();&lt;BR /&gt;#endif&lt;BR /&gt; // Set the LED to the state of "On"&lt;BR /&gt; Board_LED_Set(0, true);&lt;BR /&gt;#endif&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;// TODO: insert code here&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; FlagStatus exitflag;&lt;BR /&gt; uint8_t buffer[10];&lt;BR /&gt; int ret = 0;&lt;BR /&gt; int len;&lt;/P&gt;&lt;P&gt;SystemCoreClockUpdate();&lt;BR /&gt; //Board_Init();&lt;BR /&gt; void Board_UART_Init(LPC_USART_T *pUART)&lt;BR /&gt; {&lt;BR /&gt; Chip_SCU_PinMuxSet(0x1, 13, (SCU_MODE_PULLDOWN | SCU_MODE_FUNC1)); /* P1.13 : UART1_TXD */&lt;BR /&gt; Chip_SCU_PinMuxSet(0x1, 14, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC1)); /* P1.14 : UART1_RX */&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;Chip_UART_Init(LPC_UART);&lt;BR /&gt; Chip_UART_SetBaud(LPC_UART, 115200);&lt;BR /&gt; Chip_UART_ConfigData(LPC_UART, UART_LCR_WLEN8 | UART_LCR_SBS_1BIT); /* Default 8-N-1 */&lt;/P&gt;&lt;P&gt;/* Enable UART Transmit */&lt;BR /&gt; Chip_UART_TXEnable(LPC_UART);&lt;BR /&gt; /* Reset FIFOs, Enable FIFOs and DMA mode in UART */&lt;BR /&gt; Chip_UART_SetupFIFOS(LPC_UART, (UART_FCR_FIFO_EN | UART_FCR_RX_RS |&lt;BR /&gt; UART_FCR_TX_RS | UART_FCR_DMAMODE_SEL | UART_FCR_TRG_LEV0));&lt;/P&gt;&lt;P&gt;/* Enable UART End of Auto baudrate &amp;amp; Auto baudrate timeout interrupts */&lt;BR /&gt; Chip_UART_IntEnable(LPC_UART, (UART_IER_ABEOINT | UART_IER_ABTOINT));&lt;/P&gt;&lt;P&gt;/* preemption = 1, sub-priority = 1 */&lt;BR /&gt; NVIC_SetPriority(UARTx_IRQn, 1);&lt;BR /&gt; /* Enable Interrupt for UART0 channel */&lt;BR /&gt; NVIC_EnableIRQ(UARTx_IRQn);&lt;/P&gt;&lt;P&gt;/* Send UART Autobaud completed message */&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartABStart, sizeof(uartABStart));&lt;/P&gt;&lt;P&gt;/* ---------------------- Auto baud rate section ----------------------- */&lt;BR /&gt; /* Start auto baudrate mode */&lt;BR /&gt; Chip_UART_ABCmd(LPC_UART, UART_ACR_MODE0, true, ENABLE);&lt;/P&gt;&lt;P&gt;/* Loop until auto baudrate mode complete */&lt;BR /&gt; while (Chip_UART_GetABEOStatus(LPC_UART) == RESET) {}&lt;/P&gt;&lt;P&gt;/* Send UART Autobaud completed message */&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartABComplete, sizeof(uartABComplete));&lt;/P&gt;&lt;P&gt;/* Disable UART Interrupt */&lt;BR /&gt; NVIC_DisableIRQ(UARTx_IRQn);&lt;/P&gt;&lt;P&gt;/* Print welcome screen */&lt;BR /&gt; Print_Menu_Polling();&lt;/P&gt;&lt;P&gt;exitflag = RESET;&lt;BR /&gt; /* Read some data from the buffer */&lt;BR /&gt; while (exitflag == RESET) {&lt;BR /&gt; len = 0;&lt;BR /&gt; while (len == 0) {&lt;BR /&gt; len = Chip_UART_Read(LPC_UART, buffer, 1);&lt;BR /&gt; }&lt;BR /&gt; if (buffer[0] == 27) {&lt;BR /&gt; /* ESC key, set exit flag */&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu3, sizeof(uartPolling_menu3));&lt;BR /&gt; ret = -1;&lt;BR /&gt; exitflag = SET;&lt;BR /&gt; }&lt;BR /&gt; else if (buffer[0] == 'c') {&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu4, sizeof(uartPolling_menu4));&lt;BR /&gt; len = 0;&lt;BR /&gt; while (len == 0) {&lt;BR /&gt; len = Chip_UART_Read(LPC_UART, buffer, sizeof(buffer));&lt;BR /&gt; if ((buffer[0] != '1') &amp;amp;&amp;amp; (buffer[0] != '2') &amp;amp;&amp;amp; (buffer[0] != '3')) {&lt;BR /&gt; len = 0;&lt;BR /&gt; }&lt;BR /&gt; }&lt;BR /&gt; switch (buffer[0]) {&lt;BR /&gt; case '1': /* Polling Mode */&lt;BR /&gt; Chip_UART_SendBlocking(LPC_UART, uartPolling_menu5, sizeof(uartPolling_menu5));&lt;BR /&gt; break;&lt;/P&gt;&lt;P&gt;case '2': /* Interrupt Mode */&lt;BR /&gt; ret = 2;&lt;BR /&gt; /* Exitflag = SET; */&lt;BR /&gt; App_Interrupt_Test();&lt;BR /&gt; Print_Menu_Polling();&lt;BR /&gt; break;&lt;/P&gt;&lt;P&gt;case '3': /* DMA mode */&lt;BR /&gt; ret = 3;&lt;BR /&gt; App_DMA_Test();&lt;BR /&gt; Print_Menu_Polling();&lt;BR /&gt; break;&lt;BR /&gt; }&lt;BR /&gt; }&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;/* Wait for current transmission complete - THR must be empty */&lt;BR /&gt; while (Chip_UART_CheckBusy(LPC_UART) == SET) {}&lt;/P&gt;&lt;P&gt;/* DeInitialize UART0 peripheral */&lt;BR /&gt; Chip_UART_DeInit(LPC_UART);&lt;/P&gt;&lt;P&gt;//printf("Hello World\n", buffer[10]);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;// Force the counter to be placed into memory&lt;BR /&gt; volatile static int i = 0 ;&lt;BR /&gt; // Enter an infinite loop, just incrementing a counter&lt;BR /&gt; while(1) {&lt;BR /&gt; i++ ;&lt;BR /&gt; }&lt;BR /&gt; return 0 ;&lt;BR /&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337985"&gt;New-folder.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Dec 2016 14:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621941#M24374</guid>
      <dc:creator>nabeelfattah</dc:creator>
      <dc:date>2016-12-18T14:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: Receive Data From BLE and Printing it on LPCXpresso's consol</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621942#M24375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would be helpful if you provided an actual description of what your problem actually is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are trying to have your application display the output from printf() calls to the debugger's console view, then for LPCOpen based applications you need to make sure that your board library is configured correctly. For more details see:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/390662"&gt;LPCOpen debug input/output support&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional&amp;nbsp;information on LPCXpresso IDE's printf() support can be found at:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/389140"&gt;Using printf()&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 09:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621942#M24375</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-12-19T09:38:49Z</dc:date>
    </item>
    <item>
      <title>Re: Receive Data From BLE and Printing it on LPCXpresso's consol</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621943#M24376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is configured&amp;nbsp;correctly and I can print Hello World in the console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I need is to read data from BLE such as HC06 and print the received data in the console.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 12:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Receive-Data-From-BLE-and-Printing-it-on-LPCXpresso-s-consol/m-p/621943#M24376</guid>
      <dc:creator>nabeelfattah</dc:creator>
      <dc:date>2016-12-19T12:33:36Z</dc:date>
    </item>
  </channel>
</rss>