<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC43xx USB0 Power Domain</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621333#M24336</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have a problem. I worked on LPC4337 device powered by the USB bus. Power 3.3V produces a dc-dc converter TPS62067. Used Peripherals - USB interface, SPI and SPIFI (connected 2 SD card). Made a few dozen devices. With a fairly frequent use of the controllers have begun to fail. Namely, when the USB connection to the PC terminal.&lt;/P&gt;&lt;P&gt;I find out what goes down USB0 power domain. This domain power punches and it has a short to ground GND. Power supply to the domain through contacts and USB0_VDDA3V_DRIVER USB0_VDDA3V3. Used circuit according LPC1830_Xplorer_schematic.pdf. And if I disconnect the power from the domain of USB (desoldering ferrite), the core and the periphery of the controller function with the exception of USB interface.&lt;/P&gt;&lt;P&gt;What could be the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 18:00:47 GMT</pubDate>
    <dc:creator>dimadiman</dc:creator>
    <dc:date>2016-09-14T18:00:47Z</dc:date>
    <item>
      <title>LPC43xx USB0 Power Domain</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621333#M24336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have a problem. I worked on LPC4337 device powered by the USB bus. Power 3.3V produces a dc-dc converter TPS62067. Used Peripherals - USB interface, SPI and SPIFI (connected 2 SD card). Made a few dozen devices. With a fairly frequent use of the controllers have begun to fail. Namely, when the USB connection to the PC terminal.&lt;/P&gt;&lt;P&gt;I find out what goes down USB0 power domain. This domain power punches and it has a short to ground GND. Power supply to the domain through contacts and USB0_VDDA3V_DRIVER USB0_VDDA3V3. Used circuit according LPC1830_Xplorer_schematic.pdf. And if I disconnect the power from the domain of USB (desoldering ferrite), the core and the periphery of the controller function with the exception of USB interface.&lt;/P&gt;&lt;P&gt;What could be the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 18:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621333#M24336</guid>
      <dc:creator>dimadiman</dc:creator>
      <dc:date>2016-09-14T18:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx USB0 Power Domain</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621334#M24337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there still be the hardware circuit issue. Could you record the USB0_VDDA3V3_DRIVER &amp;amp; USB0_VDDA3V3 refer voltage 3V3 with scope? And record if the TPS62067 DC-DC converter output voltage with the same drop?&lt;/P&gt;&lt;P&gt;Please check if that voltage drop happen during USB0 module operation?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5512i2B8AA62C341C7F4A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 03:02:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621334#M24337</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-21T03:02:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx USB0 Power Domain</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621335#M24338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Voltages were tested oscilloscope in different modes . When you turn the device into a USB port , with the read and write operations are no problems .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is already asking questions how to connect the VBUS (+ 5V ) to the input USB0_VBUS controller . I have been connected directly to the USB socket USB0_VBUS contact. I believe this is the reason ! Fixed circuit and connected to the contact USB0_VBUS power from + 3.3V regulator .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the test ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 06:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-USB0-Power-Domain/m-p/621335#M24338</guid>
      <dc:creator>dimadiman</dc:creator>
      <dc:date>2016-09-22T06:47:29Z</dc:date>
    </item>
  </channel>
</rss>