<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621037#M24314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The data sheet provides absolute max rates for a scenario similar to yours (Vddio=0v) as it is specified in table 10. &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12472iBE45C458B7FEC1DE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so you shouldn't have issues if you are careful with voltage spikes when restoring the supply to the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jan 2017 00:42:01 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2017-01-25T00:42:01Z</dc:date>
    <item>
      <title>LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621036#M24313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our device is implemented with LPC 4370.&lt;BR /&gt;There is a question about the case where our device is not powered on and voltage is supplied from the target host side via the USB cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Background]&lt;BR /&gt;(1) Our device is a USB device, not a host.&lt;BR /&gt;(2) Our device is "self-powered device", not "bus-powered device".&lt;BR /&gt;(3) The other USB host device and our device are connected by a USB cable, and a voltage within the specified range is supplied to the USB cable from the USB Host device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[conditions]&lt;BR /&gt;(1) The device power supply is OFF, and the following pins of LPC4370 are not powered.&lt;/P&gt;&lt;P&gt;&amp;nbsp; VDD (IO)&lt;BR /&gt;&amp;nbsp; VDD (REG) (3 V 3)&lt;BR /&gt;&amp;nbsp; VDDA (3 V 3)&lt;BR /&gt;&amp;nbsp; USB0_VDDA3V_DRIVER&lt;BR /&gt;&amp;nbsp; USB 0 _ VDDA 3 V 3&lt;BR /&gt;&amp;nbsp; Vprog (pf)&lt;/P&gt;&lt;P&gt;(2)Voltage is applied to our device from the other host's side via the USB cable under the above conditions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;Is there a problem in applying a voltage within the specified range to the following USB pins of LPC 4370?&amp;nbsp;&lt;BR /&gt;In other words, will internal latch-up and malfunctions not occur?&lt;/P&gt;&lt;P&gt;&amp;nbsp; Pin name / specified range&lt;BR /&gt;&amp;nbsp; USB0_VBUS / min 0[V], max 3.6[V]&lt;BR /&gt;&amp;nbsp; USB0_DP / min 0[V], max 3.6[V]&lt;BR /&gt;&amp;nbsp; USB0_DM / min 0[V], max 3.6[V]&lt;BR /&gt;&amp;nbsp; USB0_ID / min 0[V], max 3.6[V]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yasushi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 09:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621036#M24313</guid>
      <dc:creator>yasushihasegawa</dc:creator>
      <dc:date>2017-01-16T09:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621037#M24314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The data sheet provides absolute max rates for a scenario similar to yours (Vddio=0v) as it is specified in table 10. &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12472iBE45C458B7FEC1DE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so you shouldn't have issues if you are careful with voltage spikes when restoring the supply to the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 00:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621037#M24314</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-01-25T00:42:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621038#M24315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Soledad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;BR /&gt;I satisfy with your answer and advice.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yasushi Hasegawa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 12:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-Is-it-possible-to-apply-a-specified-voltage-to-the-USB/m-p/621038#M24315</guid>
      <dc:creator>yasushihasegawa</dc:creator>
      <dc:date>2017-01-27T12:42:48Z</dc:date>
    </item>
  </channel>
</rss>