<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wakeup signal while in active mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wakeup-signal-while-in-active-mode/m-p/618797#M24189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It is neither of both, the Interrupt of the Signal gets into the device, but since the device it is in Active Mode, remains in the same estate.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Mar 2017 22:55:46 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2017-03-03T22:55:46Z</dc:date>
    <item>
      <title>Wakeup signal while in active mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wakeup-signal-while-in-active-mode/m-p/618796#M24188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I was checking the datasheet but i couldnt find this.&lt;/P&gt;&lt;P&gt;If lpc43xx is in active mode and a wakeup signal occurs what will happen?&lt;/P&gt;&lt;P&gt;Is the signal discarted or device reboots?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 12:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Wakeup-signal-while-in-active-mode/m-p/618796#M24188</guid>
      <dc:creator>dimitrissideris</dc:creator>
      <dc:date>2017-03-03T12:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: Wakeup signal while in active mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wakeup-signal-while-in-active-mode/m-p/618797#M24189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It is neither of both, the Interrupt of the Signal gets into the device, but since the device it is in Active Mode, remains in the same estate.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 22:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Wakeup-signal-while-in-active-mode/m-p/618797#M24189</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-03-03T22:55:46Z</dc:date>
    </item>
  </channel>
</rss>