<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54102 crashes on board init</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617624#M24147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the quick reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using LPCXpresso v8.2.2 [Build 650] [2016-09-09] on both windows 7 64bit and windows 10 64bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is preloaded with firmware in its debug probe. I tried soft loading it through the IDE and through command line and got the same results. It also supports ISP reset over debug because without it I couldn't load applications to the board when it crashes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attaching a debug log where I manually loaded the probe firmware and started a debug on a clean build of blinky&lt;/P&gt;&lt;P&gt;Jumper configuration is:&lt;/P&gt;&lt;P&gt;J1 - open&lt;/P&gt;&lt;P&gt;J2 - 1-2 (Loc)&lt;/P&gt;&lt;P&gt;J7 - 2-3 (3.3v)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 18:43:16 GMT</pubDate>
    <dc:creator>omers</dc:creator>
    <dc:date>2016-12-15T18:43:16Z</dc:date>
    <item>
      <title>LPC54102 crashes on board init</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617622#M24145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started a few days ago with an LCPXpresso54102 board and the LCPXpresso IDE. Everything went great, blinky was working and I put the board back in my drawer.&lt;/P&gt;&lt;P&gt;Today, the board was not blinking. Uploading firmware failed unless I used the ISP button.&lt;/P&gt;&lt;P&gt;After a lot of debugging I discovered that the MCU fails during board init (see attachments). I can run simple C code that does not init the board (blank c project) but an empty project that inits the board fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried deleting my workspace and starting with fresh examples, I even tried using another PC. the init keeps crashing inside Chip_Clock_SetMain_B_ClockSource&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think something is wrong with the hardware, perhaps the dreaded static damage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attachments show debugging stepping before the crash and the crash itself&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 15:28:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617622#M24145</guid>
      <dc:creator>omers</dc:creator>
      <dc:date>2016-12-15T15:28:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 crashes on board init</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617623#M24146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So what version of LPCXpresso IDE are you using with your LPCXpresso54102 board, and on what host OS? Can you provide your debug log please, as per: T&lt;A href="https://community.nxp.com/thread/389146"&gt;The Debug Log&lt;/A&gt;&amp;nbsp; ?&lt;BR /&gt; &lt;BR /&gt;Can you also confirm whether the IDE is softloading debug probe firmware into the board, or if your board has pre-programmed firmware in its debug probe? I believe that some of these boards were shipped with older probe firmware preprogrammed, and it is possible this might cause problems - in particular because it may not support &lt;A href="https://community.nxp.com/thread/389040"&gt;ISP Reset over debug&lt;/A&gt;.&amp;nbsp;&lt;BR /&gt; &lt;BR /&gt;The simplest way to ensure that the IDE is softloading is to ensure that there is a jumper fitted to the DFULink header (next to the debug probe USB port). For more info see:&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/388964"&gt;Booting LPC-Link2&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/389045"&gt;LPC-Link2 Debug Probe firmware programming&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 17:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617623#M24146</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-12-15T17:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 crashes on board init</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617624#M24147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the quick reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using LPCXpresso v8.2.2 [Build 650] [2016-09-09] on both windows 7 64bit and windows 10 64bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is preloaded with firmware in its debug probe. I tried soft loading it through the IDE and through command line and got the same results. It also supports ISP reset over debug because without it I couldn't load applications to the board when it crashes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attaching a debug log where I manually loaded the probe firmware and started a debug on a clean build of blinky&lt;/P&gt;&lt;P&gt;Jumper configuration is:&lt;/P&gt;&lt;P&gt;J1 - open&lt;/P&gt;&lt;P&gt;J2 - 1-2 (Loc)&lt;/P&gt;&lt;P&gt;J7 - 2-3 (3.3v)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 18:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617624#M24147</guid>
      <dc:creator>omers</dc:creator>
      <dc:date>2016-12-15T18:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 crashes on board init</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617625#M24148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything else I can try or all hope was lost with this board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 09:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617625#M24148</guid>
      <dc:creator>omers</dc:creator>
      <dc:date>2016-12-22T09:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 crashes on board init</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617626#M24149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&amp;nbsp;Maybe &lt;STRONG&gt;TRY&lt;/STRONG&gt;&amp;nbsp;change&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt; #define BOARD_MAINCLOCKRATE &amp;nbsp; &amp;nbsp; (100000000) &amp;nbsp; //100Mhz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;to&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&lt;SPAN&gt;#define BOARD_MAINCLOCKRATE &amp;nbsp; &amp;nbsp; (96000000) &amp;nbsp; //&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 14:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-crashes-on-board-init/m-p/617626#M24149</guid>
      <dc:creator>okcn</dc:creator>
      <dc:date>2016-12-23T14:34:29Z</dc:date>
    </item>
  </channel>
</rss>