<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Om13085 code not executing/starting after Reset</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Om13085-code-not-executing-starting-after-Reset/m-p/617033#M24117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you also posted this question as response to a previous thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/435247?sr=stream"&gt;https://community.nxp.com/thread/435247?sr=stream&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since I answered that one, I am marking this thread as assumed answered too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Brendon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 18:54:09 GMT</pubDate>
    <dc:creator>brendonslade</dc:creator>
    <dc:date>2016-12-15T18:54:09Z</dc:date>
    <item>
      <title>Om13085 code not executing/starting after Reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Om13085-code-not-executing-starting-after-Reset/m-p/617032#M24116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I´m using the the OM13085 and somehow the code is only executing when connected to the IDE/debugger and right after the firmware have been flashed.&lt;/P&gt;&lt;P&gt;If I reset the board or switch it off and on the code is not executing...&lt;/P&gt;&lt;P&gt;My project is based on the uIP/webserver samples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;br Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 13:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Om13085-code-not-executing-starting-after-Reset/m-p/617032#M24116</guid>
      <dc:creator>ronwal</dc:creator>
      <dc:date>2016-12-15T13:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: Om13085 code not executing/starting after Reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Om13085-code-not-executing-starting-after-Reset/m-p/617033#M24117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you also posted this question as response to a previous thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/435247?sr=stream"&gt;https://community.nxp.com/thread/435247?sr=stream&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since I answered that one, I am marking this thread as assumed answered too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Brendon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 18:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Om13085-code-not-executing-starting-after-Reset/m-p/617033#M24117</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2016-12-15T18:54:09Z</dc:date>
    </item>
  </channel>
</rss>