<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: The question of LPC2929</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-question-of-LPC2929/m-p/615533#M24059</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC2929 operates in normal-power mode after reset. In this mode the device is fully functional. The system can be put into idle-power mode either partially or fully.&lt;BR /&gt;LPC2929 contains external reset input and internal power-up reset circuits. This ensures that a reset is internally extended internally until the oscillators and flash have reached a stable state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC2929 has 768kB flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jan 2017 07:55:43 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-01-30T07:55:43Z</dc:date>
    <item>
      <title>The question of LPC2929</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-question-of-LPC2929/m-p/615532#M24058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1、I would like to ask does this ARM9 LPC2929 chip have on the power sequence requirements?&lt;/P&gt;&lt;P&gt;2、If I want to use a LPC2929 plug-in FLASH, I would like to ask at least how much FLASH?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 07:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-question-of-LPC2929/m-p/615532#M24058</guid>
      <dc:creator>1263906294</dc:creator>
      <dc:date>2017-01-13T07:54:19Z</dc:date>
    </item>
    <item>
      <title>Re: The question of LPC2929</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-question-of-LPC2929/m-p/615533#M24059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC2929 operates in normal-power mode after reset. In this mode the device is fully functional. The system can be put into idle-power mode either partially or fully.&lt;BR /&gt;LPC2929 contains external reset input and internal power-up reset circuits. This ensures that a reset is internally extended internally until the oscillators and flash have reached a stable state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC2929 has 768kB flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 07:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-question-of-LPC2929/m-p/615533#M24059</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-01-30T07:55:43Z</dc:date>
    </item>
  </channel>
</rss>