<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC3250 access sdram in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3250-access-sdram/m-p/615089#M24048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could refer to application note &lt;A href="http://www.nxp.com/documents/application_note/AN10935.pdf"&gt;AN10935 “Using SDR/DDR SDRAM memories with LPC32xx”&lt;/A&gt; in order to verify the connections of your SDRAM modules to the LPC microcontroller.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Dec 2016 21:49:23 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2016-12-05T21:49:23Z</dc:date>
    <item>
      <title>LPC3250 access sdram</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3250-access-sdram/m-p/615088#M24047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two 16M x 16 SDRAM connect to the LPC3250 as a 32bit wide SDRAM.&lt;/P&gt;&lt;P&gt;I get some problems when accessing the SDRAM.&lt;/P&gt;&lt;P&gt;When write:&lt;/P&gt;&lt;P&gt;UNS_32 *p = (UNS_32 *)0x83FC0000;&lt;/P&gt;&lt;P&gt;*p = 0xE59F002C;&lt;/P&gt;&lt;P&gt;Then read from &lt;EM&gt;p&lt;/EM&gt; and &lt;EM&gt;p+4, and &lt;/EM&gt;the result is 0xE59FE59F, 0x002C002C&lt;EM&gt; &lt;/EM&gt;respectively&lt;EM&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I cannot figure out what is wrong.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 15:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3250-access-sdram/m-p/615088#M24047</guid>
      <dc:creator>ywzhu</dc:creator>
      <dc:date>2016-11-22T15:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC3250 access sdram</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3250-access-sdram/m-p/615089#M24048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could refer to application note &lt;A href="http://www.nxp.com/documents/application_note/AN10935.pdf"&gt;AN10935 “Using SDR/DDR SDRAM memories with LPC32xx”&lt;/A&gt; in order to verify the connections of your SDRAM modules to the LPC microcontroller.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 21:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3250-access-sdram/m-p/615089#M24048</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-12-05T21:49:23Z</dc:date>
    </item>
  </channel>
</rss>