<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Using GPIO to simulate I2C?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-GPIO-to-simulate-I2C/m-p/613962#M24010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is that possible to use GPIO to simulate I2C in LPC18xx? It seem NXP don't allow the GPIO to be configured as both input and output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2017 04:00:20 GMT</pubDate>
    <dc:creator>lidouhe</dc:creator>
    <dc:date>2017-03-02T04:00:20Z</dc:date>
    <item>
      <title>Using GPIO to simulate I2C?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-GPIO-to-simulate-I2C/m-p/613962#M24010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is that possible to use GPIO to simulate I2C in LPC18xx? It seem NXP don't allow the GPIO to be configured as both input and output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 04:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-GPIO-to-simulate-I2C/m-p/613962#M24010</guid>
      <dc:creator>lidouhe</dc:creator>
      <dc:date>2017-03-02T04:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: Using GPIO to simulate I2C?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-GPIO-to-simulate-I2C/m-p/613963#M24011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lidou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPC18xx contains the below features that you can use:&lt;/P&gt;&lt;P&gt;– One Fast-mode Plus I2C-bus interface with monitor mode and with open-drain I/O pins conforming to the full I2C-bus specification. Supports data rates of up to 1 Mbit/s.&lt;/P&gt;&lt;P&gt;– One standard I2C-bus interface with monitor mode and standard I/O pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However,&amp;nbsp; it is possible to implement a GPIO to simulate I2C, but you need to create your own algorithm and change the pin configuration between output and input every time you need.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Sol &lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 20:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-GPIO-to-simulate-I2C/m-p/613963#M24011</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-03-06T20:12:35Z</dc:date>
    </item>
  </channel>
</rss>