<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ethernet on hitex 4350 eval board in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ethernet-on-hitex-4350-eval-board/m-p/613680#M23994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I am trying to run sa_tcpecho-spifi_hitex_eva_4350 example on Hitex 4350 eval board. This is an example&lt;BR /&gt; with lwIP stack without an RTOS, provided by LPCOPEN. I selected MII interface.&lt;BR /&gt;I checked all jumper setting required for etehernet as described in "Quickstart_LPC1850EVA-LPC4350-A4.pdf".&lt;BR /&gt;I set a static IP address on the code. &lt;BR /&gt;When I plug in a ethernet cable the code realize the event, but when I make a ping to that IP address &lt;BR /&gt;I have no response.&lt;BR /&gt;The example doesn't work. Is there any specific setting that need to be done in the code or on the hitex &lt;BR /&gt;eval board to make the ethernet work?&lt;BR /&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2017 10:04:52 GMT</pubDate>
    <dc:creator>Icio</dc:creator>
    <dc:date>2017-02-08T10:04:52Z</dc:date>
    <item>
      <title>ethernet on hitex 4350 eval board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ethernet-on-hitex-4350-eval-board/m-p/613680#M23994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I am trying to run sa_tcpecho-spifi_hitex_eva_4350 example on Hitex 4350 eval board. This is an example&lt;BR /&gt; with lwIP stack without an RTOS, provided by LPCOPEN. I selected MII interface.&lt;BR /&gt;I checked all jumper setting required for etehernet as described in "Quickstart_LPC1850EVA-LPC4350-A4.pdf".&lt;BR /&gt;I set a static IP address on the code. &lt;BR /&gt;When I plug in a ethernet cable the code realize the event, but when I make a ping to that IP address &lt;BR /&gt;I have no response.&lt;BR /&gt;The example doesn't work. Is there any specific setting that need to be done in the code or on the hitex &lt;BR /&gt;eval board to make the ethernet work?&lt;BR /&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 10:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ethernet-on-hitex-4350-eval-board/m-p/613680#M23994</guid>
      <dc:creator>Icio</dc:creator>
      <dc:date>2017-02-08T10:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: ethernet on hitex 4350 eval board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ethernet-on-hitex-4350-eval-board/m-p/613681#M23995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maurizio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below thread and let me know if this helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/418220"&gt;LwIP sample fail&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 23:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ethernet-on-hitex-4350-eval-board/m-p/613681#M23995</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-02-14T23:33:35Z</dc:date>
    </item>
  </channel>
</rss>