<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックadc_8xx.h trigger sources in SEQ_CTRL</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612204#M23937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working about a LPC824. In order to use the ADC with LPCOPEN I have to trigger it with the SCT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time, adc_8xx.h macro in "ADC hardware trigger sourcers in SEQ_CTRL" are 11 items. These 11 items aren't like the ADC hardware trigger inputs (Table276. ADC hardware trigger inputs) in UM10800.pdf. These item aren't similiar at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am confused. Is the macro other thing?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks so much and regards. Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Mar 2017 17:54:27 GMT</pubDate>
    <dc:creator>vaque</dc:creator>
    <dc:date>2017-03-23T17:54:27Z</dc:date>
    <item>
      <title>adc_8xx.h trigger sources in SEQ_CTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612204#M23937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working about a LPC824. In order to use the ADC with LPCOPEN I have to trigger it with the SCT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time, adc_8xx.h macro in "ADC hardware trigger sourcers in SEQ_CTRL" are 11 items. These 11 items aren't like the ADC hardware trigger inputs (Table276. ADC hardware trigger inputs) in UM10800.pdf. These item aren't similiar at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am confused. Is the macro other thing?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks so much and regards. Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 17:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612204#M23937</guid>
      <dc:creator>vaque</dc:creator>
      <dc:date>2017-03-23T17:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: adc_8xx.h trigger sources in SEQ_CTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612205#M23938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="296398" data-username="vaque" href="https://community.nxp.com/people/vaque"&gt;Daniel Vaquerizo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Firstly, the Table 276 exemplifies the correct hardware trigger inputs, you can ignore the interference as LPCOpen library is designed for all kinds of LPC MCU, and the LPCOpen for the LPCXpresso 824 would inherit&amp;nbsp; all macro certainly.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 02:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612205#M23938</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2017-03-24T02:02:29Z</dc:date>
    </item>
    <item>
      <title>Re: adc_8xx.h trigger sources in SEQ_CTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612206#M23939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok. Thanks. &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Have a great day too&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards. Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 10:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/adc-8xx-h-trigger-sources-in-SEQ-CTRL/m-p/612206#M23939</guid>
      <dc:creator>vaque</dc:creator>
      <dc:date>2017-03-24T10:11:00Z</dc:date>
    </item>
  </channel>
</rss>