<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Configure PWM channels using SCT in LPC1549</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513580#M239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ramniraj10 on Tue Aug 12 22:36:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1. LPC15XX.pdf: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Configurable PWM/timer/motor control subsystem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to four 32-bit counter/timers or up to eight 16-bit counter/timers or combinations&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of 16-bit and 32-bit timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to 28 match outputs and 22 configurable capture inputs with input multiplexer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to 28 PWM outputs total.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. UM10736.pdf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a) page 222&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Counters can be used in conjunction with match registers to toggle outputs and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;create time-proportioned PWM signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Up to 8 single-edge or dual-edge controlled PWM outputs with independent duty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;cycles and common PWM cycle length.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;b) page 223&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;10 outputs (some outputs are connected to multiple locations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as movable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Five outputs connected to external pins through the switch matrix as fixed-pin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to the SCTIPU to use as sample and abort inputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– One output connected to the other large SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Four outputs connected to one small SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to each ADC trigger input&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;c) page 268&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Counters can be used in conjunction with match registers to toggle outputs and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;create time-proportioned PWM signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Up to six single-edge or dual-edge controlled PWM outputs with independent duty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;cycles if configured as 32-bit timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;d) page 269&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;6 outputs (some outputs are connected to multiple locations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as movable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as fixed-pin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to the SCT IPU to use as sample and abort inputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Four outputs connected to the accompanying large SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to each ADC trigger input&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;From above points, total PWM outputs possible according to LPC15XX.pdf is 28.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and according to UM10736.pdf, total possible = a +b+c+d = 8+8+6+6 = 28.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But, i doubt if it is possible or not because my project and micro controller selection is based on this query.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:07:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:07:45Z</dc:date>
    <item>
      <title>Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513577#M236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ramniraj10 on Sun Aug 10 23:37:54 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to configure 27 PWM channels using SCT timer in LPC1549?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you provide initialization routine or state machine diagram for the same?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513577#M236</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513578#M237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by YOZHik on Tue Aug 12 13:56:12 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No. SCT0 and SCT1 have 7 outputs available on external pins each. SCT2 and SCT3 have 6 outputs available on external pins each. Therefore a theoretical maximum is 7+7+6+6=26 externally available PWM outputs.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513578#M237</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513579#M238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LabRat on Tue Aug 12 14:49:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: YOZHik&lt;/STRONG&gt;&lt;BR /&gt;No. SCT0 and SCT1 have 7 outputs available on external pins each..&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;8&amp;nbsp; at LQFP100 :) &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513579#M238</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513580#M239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ramniraj10 on Tue Aug 12 22:36:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1. LPC15XX.pdf: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Configurable PWM/timer/motor control subsystem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to four 32-bit counter/timers or up to eight 16-bit counter/timers or combinations&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of 16-bit and 32-bit timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to 28 match outputs and 22 configurable capture inputs with input multiplexer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Up to 28 PWM outputs total.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. UM10736.pdf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a) page 222&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Counters can be used in conjunction with match registers to toggle outputs and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;create time-proportioned PWM signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Up to 8 single-edge or dual-edge controlled PWM outputs with independent duty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;cycles and common PWM cycle length.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;b) page 223&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;10 outputs (some outputs are connected to multiple locations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as movable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Five outputs connected to external pins through the switch matrix as fixed-pin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to the SCTIPU to use as sample and abort inputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– One output connected to the other large SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Four outputs connected to one small SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to each ADC trigger input&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;c) page 268&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Counters can be used in conjunction with match registers to toggle outputs and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;create time-proportioned PWM signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Up to six single-edge or dual-edge controlled PWM outputs with independent duty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;cycles if configured as 32-bit timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;d) page 269&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;6 outputs (some outputs are connected to multiple locations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as movable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Three outputs connected to external pins through the switch matrix as fixed-pin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to the SCT IPU to use as sample and abort inputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Four outputs connected to the accompanying large SCT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– Two outputs connected to each ADC trigger input&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;From above points, total PWM outputs possible according to LPC15XX.pdf is 28.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and according to UM10736.pdf, total possible = a +b+c+d = 8+8+6+6 = 28.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But, i doubt if it is possible or not because my project and micro controller selection is based on this query.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513580#M239</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513581#M240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LabRat on Wed Aug 13 03:52:45 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: ramniraj10&lt;/STRONG&gt;&lt;BR /&gt;But, i doubt if it is possible...&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So what's not clear there? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just use LQFP100 and start with sample 'periph_sct_pwm' ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513581#M240</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:46Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513582#M241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Thu Aug 14 17:21:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi ramniraj1,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In LQFP100 package, all 28 PWMs are available at the pins. Although SCT0 and SCT1 has 10 outputs each, all of them are not coming out to pins. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See below break-up. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SCT0&amp;nbsp; -&amp;gt; (Out0 to Out7)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; 8 Outputs&amp;nbsp;&amp;nbsp; connected to pins&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SCT1 -&amp;gt; (Out0 to Out7)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; 8 Outputs&amp;nbsp;&amp;nbsp; connected to pins&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SCT2&amp;nbsp; -&amp;gt; (Out0 to Out5)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; 6 Outputs&amp;nbsp;&amp;nbsp; connected to pins&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SCT3&amp;nbsp; -&amp;gt; (Out0 to Out5)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; 6 Outputs&amp;nbsp;&amp;nbsp; connected to pins&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Total SCT outputs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; 8+8+6+6 =28&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; connected to pins&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513582#M241</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:46Z</dc:date>
    </item>
    <item>
      <title>Re: Configure PWM channels using SCT in LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513583#M242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ramniraj10 on Wed Aug 20 01:53:35 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear MC,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your suggestion. :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Configure-PWM-channels-using-SCT-in-LPC1549/m-p/513583#M242</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:07:47Z</dc:date>
    </item>
  </channel>
</rss>