<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPCXpresso board LPC812  periph_uart example</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-board-LPC812-periph-uart-example/m-p/611436#M23884</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for your input :smileywink:&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Mar 2017 00:28:11 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2017-03-23T00:28:11Z</dc:date>
    <item>
      <title>LPCXpresso board LPC812  periph_uart example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-board-LPC812-periph-uart-example/m-p/611435#M23883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am able to get the&amp;nbsp; periph_uart example to run, the leds blink, however the board is not outputting anything&lt;/P&gt;&lt;P&gt;on the serial port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Things done:&lt;/P&gt;&lt;P&gt;Soldered a header into J7, and wired a USB to serial cable (one I have used on a cubieboard)&lt;/P&gt;&lt;P&gt;Confirmed the serial cable is working by tying Tx and Rx together&lt;/P&gt;&lt;P&gt;Black wire from usb cable to board ground&lt;/P&gt;&lt;P&gt;White wire from usb cable to LPC812 PIO0_0, Tx&lt;/P&gt;&lt;P&gt;Green wire from usb cable to LPC812 PIO0_4, Rx&lt;/P&gt;&lt;P&gt;Set the baud rate to 115200 in both Windows device manager, and putty terminal&lt;/P&gt;&lt;P&gt;I have not made any changes to the example project. Project is from LPSOpen.&lt;/P&gt;&lt;P&gt;LPCXpresso v8.2.2 [Build 650] [2016-09-09]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thought maybe it was not possible to use the board's uart while in debug mode, so I built and tried a release version,&lt;/P&gt;&lt;P&gt;but had the same negative result. Any thoughts would be appreciated. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;... Two minutes after posting this I swapped Rx and Tx connections and it worked. I had hesitated to try this because&lt;/P&gt;&lt;P&gt;I was sure the wiring was ok, same as on cubieboard, and I was afraid of damaging the board. However, after checking&lt;/P&gt;&lt;P&gt;there pdf schematic, there are are 220 ohm resistors in series with the pins so I went ahead and swapped the wires.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 22:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-board-LPC812-periph-uart-example/m-p/611435#M23883</guid>
      <dc:creator>walt_lpc</dc:creator>
      <dc:date>2017-03-22T22:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso board LPC812  periph_uart example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-board-LPC812-periph-uart-example/m-p/611436#M23884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for your input :smileywink:&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 00:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-board-LPC812-periph-uart-example/m-p/611436#M23884</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-03-23T00:28:11Z</dc:date>
    </item>
  </channel>
</rss>