<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54102 - Do the timers require interrupts to trigger DMA transfers, or a match with a chosen value is enough?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/611086#M23866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with LPC54102 to transfer data from certain buffers to the GPIO outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The time is critical and I do not need interrupts each time a DMA transfer needs to be triggered.&lt;/P&gt;&lt;P&gt;Is it enough to program a timer (that can trigger a DMA channel) with a match value, and each time the TC will match that value a flag will trigger the DMA without interrupting (and going into the ISR in order to clear the interrupt)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would really appreciate your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Doini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Sep 2016 21:40:48 GMT</pubDate>
    <dc:creator>doini</dc:creator>
    <dc:date>2016-09-12T21:40:48Z</dc:date>
    <item>
      <title>LPC54102 - Do the timers require interrupts to trigger DMA transfers, or a match with a chosen value is enough?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/611086#M23866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with LPC54102 to transfer data from certain buffers to the GPIO outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The time is critical and I do not need interrupts each time a DMA transfer needs to be triggered.&lt;/P&gt;&lt;P&gt;Is it enough to program a timer (that can trigger a DMA channel) with a match value, and each time the TC will match that value a flag will trigger the DMA without interrupting (and going into the ISR in order to clear the interrupt)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would really appreciate your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Doini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 21:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/611086#M23866</guid>
      <dc:creator>doini</dc:creator>
      <dc:date>2016-09-12T21:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 - Do the timers require interrupts to trigger DMA transfers, or a match with a chosen value is enough?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/611087#M23867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Doini&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you ever get this figured out? I&amp;nbsp;am doing the same thing. I believe that there should be no interrupt necessary and that the match should be able to trigger the DMA unrelated to the exernal match pins. I have not been able to get this to work but I think that I am close. I posted a question about this including my LPCOpen code yesterday called "Cannot get DMA triggered with Timer Match".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good Luck - James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 16:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/611087#M23867</guid>
      <dc:creator>jamesm</dc:creator>
      <dc:date>2016-10-18T16:39:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54102 - Do the timers require interrupts to trigger DMA transfers, or a match with a chosen v</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/1733960#M54270</link>
      <description>did you guys figure it out ? haha</description>
      <pubDate>Wed, 04 Oct 2023 21:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54102-Do-the-timers-require-interrupts-to-trigger-DMA/m-p/1733960#M54270</guid>
      <dc:creator>skanda19</dc:creator>
      <dc:date>2023-10-04T21:31:20Z</dc:date>
    </item>
  </channel>
</rss>