<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4370 HSADC clocking issues in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609219#M23759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just have discovered that the HSADC of the LPC4370 generates a big amount of interference noise when I use the Audio-PLL as clock source. When I use the Main-PLL the noise is completely gone.&lt;/P&gt;&lt;P&gt;Setup:&lt;/P&gt;&lt;P&gt;Audio-PLL running at 460.8 MHz&lt;/P&gt;&lt;P&gt;Main-PLL running at 204MHz&lt;/P&gt;&lt;P&gt;HSADC sample rate is 1536kHz.&lt;/P&gt;&lt;P&gt;Result: Interference noise (~9.6kHz) (synchronous) (1536/160) with a level of&amp;nbsp; +/- 200 digits = 10% of conversion range!!!&lt;/P&gt;&lt;P&gt;If I run the HSADC with a clock that is derived from the main-pll with a frequency of 1545,45 kHz, the interference noise is gone.&lt;/P&gt;&lt;P&gt;In my application I have to sample a signal quasi synchronously - which is not possible, when I use the main-pll.&lt;/P&gt;&lt;P&gt;Any suggestions what can be done - or is it simple a hw-limitation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-Otto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Nov 2016 21:32:04 GMT</pubDate>
    <dc:creator>franz-ottowitte</dc:creator>
    <dc:date>2016-11-20T21:32:04Z</dc:date>
    <item>
      <title>LPC4370 HSADC clocking issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609219#M23759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just have discovered that the HSADC of the LPC4370 generates a big amount of interference noise when I use the Audio-PLL as clock source. When I use the Main-PLL the noise is completely gone.&lt;/P&gt;&lt;P&gt;Setup:&lt;/P&gt;&lt;P&gt;Audio-PLL running at 460.8 MHz&lt;/P&gt;&lt;P&gt;Main-PLL running at 204MHz&lt;/P&gt;&lt;P&gt;HSADC sample rate is 1536kHz.&lt;/P&gt;&lt;P&gt;Result: Interference noise (~9.6kHz) (synchronous) (1536/160) with a level of&amp;nbsp; +/- 200 digits = 10% of conversion range!!!&lt;/P&gt;&lt;P&gt;If I run the HSADC with a clock that is derived from the main-pll with a frequency of 1545,45 kHz, the interference noise is gone.&lt;/P&gt;&lt;P&gt;In my application I have to sample a signal quasi synchronously - which is not possible, when I use the main-pll.&lt;/P&gt;&lt;P&gt;Any suggestions what can be done - or is it simple a hw-limitation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-Otto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Nov 2016 21:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609219#M23759</guid>
      <dc:creator>franz-ottowitte</dc:creator>
      <dc:date>2016-11-20T21:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 HSADC clocking issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609220#M23760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you tried using the USB PLL?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 16:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609220#M23760</guid>
      <dc:creator>hairy_lee</dc:creator>
      <dc:date>2016-11-24T16:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 HSADC clocking issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609221#M23761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB clock must be multiple of 48MHz as I am using USB. That's a no-go.&lt;/P&gt;&lt;P&gt;My question was - is the HSADC not usable if the supplied clock is not a direct divsor the the main-pll clock due to interference noise?&amp;nbsp;&lt;BR /&gt;If this is the case - at least a note in the UM should be given.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 20:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609221#M23761</guid>
      <dc:creator>franz-ottowitte</dc:creator>
      <dc:date>2016-11-24T20:55:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 HSADC clocking issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609222#M23762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe it is a configuration issue, please check the following thread, this may helps.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.lpcware.com/content/forum/lpc4370-acdhs-speed" title="https://www.lpcware.com/content/forum/lpc4370-acdhs-speed"&gt;LPC4370 ACDHS speed | www.LPCware.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 18:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-clocking-issues/m-p/609222#M23762</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-12-28T18:26:48Z</dc:date>
    </item>
  </channel>
</rss>