<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lwIP port to LPC2478 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517850#M2369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tamirmichael on Wed Sep 05 03:21:09 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have correctly setup the peripheral pins, ISR etc.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:29:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:29:52Z</dc:date>
    <item>
      <title>lwIP port to LPC2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517849#M2368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tamirmichael on Wed Sep 05 03:17:39 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to port the available lwIP port for LPC17xx devices (BTW thanks for fixing it recently!) to a LPC2478. However, my program crashes and I know it is due to the device driver. I thought the Ethernet blocks of the LPC2478 and LPC1788 were identical (is that true?). I have forgotten something, but I would really appreciate if somebody helped me out...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517849#M2368</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: lwIP port to LPC2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517850#M2369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tamirmichael on Wed Sep 05 03:21:09 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have correctly setup the peripheral pins, ISR etc.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517850#M2369</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: lwIP port to LPC2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517851#M2370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wellsk on Wed Sep 05 08:49:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The blocks are the same IP, but clocking and usable memory for descriptors/buffers will vary per device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would think the 17xx driver would work on the 24xx and 32xx devices that use the same IP with some small changes which it sounds like you made.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are hitting an LWIP assertion, can you post it here?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If it's a crash, that's a bit harder to debug.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does it crash when the Ethernet cable is not plugged in? Or just when you try to send or receive a packet?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517851#M2370</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: lwIP port to LPC2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517852#M2371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tamirmichael on Thu Sep 06 02:02:10 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I managed to get it to work - DHCP is working, now i'm going to compare large file upload speed with LPC1788.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem was a combination of stack sizes, ethernet initialization code (I used my own - replaced by your Cortex M3 port) etc. ! I also imported the memory mapped IO approach of the LPC1788 to the LPC2478 to ease the reuse of the network driver.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lwIP-port-to-LPC2478/m-p/517852#M2371</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:54Z</dc:date>
    </item>
  </channel>
</rss>