<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605128#M23579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David Atkins&lt;/P&gt;&lt;P&gt;Land &amp;amp; Naval Defence Electronics Division&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leonardo MW Ltd&lt;/P&gt;&lt;P&gt;20A1-2 Ground Floor Southside PO Box 5&lt;/P&gt;&lt;P&gt;Southmead Road&lt;/P&gt;&lt;P&gt;Filton&lt;/P&gt;&lt;P&gt;Bristol&lt;/P&gt;&lt;P&gt;BS34 7QW&lt;/P&gt;&lt;P&gt;david.atkins@leonardocompany.com&amp;lt;mailto:david.atkins@leonardocompany.com&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tel: +44 (0) 117 931 3556&lt;/P&gt;&lt;P&gt;Mob: +44 (0) 7793422675&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HELICOPTERS / AERONAUTICS / ELECTRONICS, DEFENCE AND SECURITY SYSTEMS / SPACE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Feb 2017 20:56:24 GMT</pubDate>
    <dc:creator>atkinsd84</dc:creator>
    <dc:date>2017-02-07T20:56:24Z</dc:date>
    <item>
      <title>What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605126#M23577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, I'm struggling with how to terminate unused pins and the data sheet doesn't appear to have all the answers.&amp;nbsp; Can anyone help me with how to terminate pins 16 and 18 on the LPC1768 when not using the RTC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 15:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605126#M23577</guid>
      <dc:creator>atkinsd84</dc:creator>
      <dc:date>2017-02-06T15:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605127#M23578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;I would recommend that RTCX1 be grounded since it is an input. RTCX2 is an output, so it can be left open.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 20:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605127#M23578</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-02-07T20:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605128#M23579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David Atkins&lt;/P&gt;&lt;P&gt;Land &amp;amp; Naval Defence Electronics Division&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leonardo MW Ltd&lt;/P&gt;&lt;P&gt;20A1-2 Ground Floor Southside PO Box 5&lt;/P&gt;&lt;P&gt;Southmead Road&lt;/P&gt;&lt;P&gt;Filton&lt;/P&gt;&lt;P&gt;Bristol&lt;/P&gt;&lt;P&gt;BS34 7QW&lt;/P&gt;&lt;P&gt;david.atkins@leonardocompany.com&amp;lt;mailto:david.atkins@leonardocompany.com&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tel: +44 (0) 117 931 3556&lt;/P&gt;&lt;P&gt;Mob: +44 (0) 7793422675&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HELICOPTERS / AERONAUTICS / ELECTRONICS, DEFENCE AND SECURITY SYSTEMS / SPACE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 20:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-do-I-do-with-the-RTCX1-and-RTCX2-pins-when-not-using-the/m-p/605128#M23579</guid>
      <dc:creator>atkinsd84</dc:creator>
      <dc:date>2017-02-07T20:56:24Z</dc:date>
    </item>
  </channel>
</rss>