<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 4xCAN + USB + Automotive? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604898#M23566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;has there been any news in the meantime? The requirement for a current project would be:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- CAN-FD support&lt;/P&gt;&lt;P&gt;&amp;nbsp;- USB&lt;/P&gt;&lt;P&gt;&amp;nbsp;- ARM-Cortex&lt;/P&gt;&lt;P&gt;&amp;nbsp;- LQFP 48-100&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Flash size 128kB+&lt;/P&gt;&lt;P&gt;How can I select in the NXP product selector CAN-FD, there is no option? Or did I oversee something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks + best regards, Rainer&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 11:15:15 GMT</pubDate>
    <dc:creator>rka</dc:creator>
    <dc:date>2018-02-22T11:15:15Z</dc:date>
    <item>
      <title>4xCAN + USB + Automotive?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604896#M23564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently I use the LPC1756 with USB and CAN to send and receive data to a Windows application. For this purpose, an very reliable driver solution exists and a bootloader enables encrypted firmware updates using nice windows applications.&lt;/P&gt;&lt;P&gt;I want to reuse as many as possible existing source.&lt;/P&gt;&lt;P&gt;For a new project, the microcontroller must be automotive specified, have 4 CAN units and best a LQFP48-80 case. Unfortunately I cannot find a matching microcontroller with additional USB.&lt;/P&gt;&lt;P&gt;Of course a small LPC or FTDI could be added or CAN used for firmware updates, but I would like to omit unnecessary complexity. Customers should be able to do configuration or updates directly using a PC or laptop.&lt;/P&gt;&lt;P&gt;Ideas or tips which microcontroller to use are welcome.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best, Rainer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 21:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604896#M23564</guid>
      <dc:creator>rka</dc:creator>
      <dc:date>2017-01-10T21:10:59Z</dc:date>
    </item>
    <item>
      <title>Re: 4xCAN + USB + Automotive?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604897#M23565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rainer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a quick check and I believe that we do not have a MCU with all the features that you request on the same chip.&lt;/P&gt;&lt;P&gt;we will launch the S32K that will have up to 6 CAN but this device do not have USB module, maybe you can use a UART instead of the USB adding a USB to serial.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/s32-arm-processors-microcontrollers/32-bit-automotive-general-purpose-microcontrollers:S32K" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/s32-arm-processors-microcontrollers/32-bit-automotive-general-purpose-microcontrollers:S32K"&gt;32-bit Automotive General Purpose MCUs|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 21:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604897#M23565</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2017-01-12T21:49:04Z</dc:date>
    </item>
    <item>
      <title>Re: 4xCAN + USB + Automotive?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604898#M23566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;has there been any news in the meantime? The requirement for a current project would be:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- CAN-FD support&lt;/P&gt;&lt;P&gt;&amp;nbsp;- USB&lt;/P&gt;&lt;P&gt;&amp;nbsp;- ARM-Cortex&lt;/P&gt;&lt;P&gt;&amp;nbsp;- LQFP 48-100&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Flash size 128kB+&lt;/P&gt;&lt;P&gt;How can I select in the NXP product selector CAN-FD, there is no option? Or did I oversee something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks + best regards, Rainer&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 11:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4xCAN-USB-Automotive/m-p/604898#M23566</guid>
      <dc:creator>rka</dc:creator>
      <dc:date>2018-02-22T11:15:15Z</dc:date>
    </item>
  </channel>
</rss>