<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4357 Can I use a timer during changing clock.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-Can-I-use-a-timer-during-changing-clock/m-p/604656#M23546</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Iwao Mizota,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, if you like, you can use the timer to wait the PLL1 to lock instead of using the while to wait.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; But one point you should take care, the chapter you mentioned, is using the IRC as the BASE_M4_CLK source, and this BASE_M4_CLK also the timer's(Timer0/1/2/3) base clock.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You should make sure when the timer is working, the BASE_M4_CLK is not changed. You should disable the timer before you select the PLL1 as the BASE_M4_CLK source.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 09:02:20 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-11-21T09:02:20Z</dc:date>
    <item>
      <title>LPC4357 Can I use a timer during changing clock.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-Can-I-use-a-timer-during-changing-clock/m-p/604655#M23545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Could please tell me whether I can use time on STEP5 of below sequence on LPC4357.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 9 STEP on chapter 13.2.2.1 of UM10503&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;STEP5: wait for the PLL1 to lock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to make a code to&amp;nbsp;detect when it is long time to lock PLL1.&lt;/P&gt;&lt;P&gt;And system go back to work on internal clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bet Regards.&lt;/P&gt;&lt;P&gt;Iwao Mizota.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Nov 2016 00:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-Can-I-use-a-timer-during-changing-clock/m-p/604655#M23545</guid>
      <dc:creator>iwaomizota</dc:creator>
      <dc:date>2016-11-18T00:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 Can I use a timer during changing clock.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-Can-I-use-a-timer-during-changing-clock/m-p/604656#M23546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Iwao Mizota,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, if you like, you can use the timer to wait the PLL1 to lock instead of using the while to wait.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; But one point you should take care, the chapter you mentioned, is using the IRC as the BASE_M4_CLK source, and this BASE_M4_CLK also the timer's(Timer0/1/2/3) base clock.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You should make sure when the timer is working, the BASE_M4_CLK is not changed. You should disable the timer before you select the PLL1 as the BASE_M4_CLK source.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 09:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-Can-I-use-a-timer-during-changing-clock/m-p/604656#M23546</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-11-21T09:02:20Z</dc:date>
    </item>
  </channel>
</rss>