<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Bit band mapping on LPC5410x</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604344#M23541</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x&amp;nbsp;Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.&lt;/P&gt;&lt;P&gt;This means all the APB Peripherals are mapped in the bit-band region.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 21:30:53 GMT</pubDate>
    <dc:creator>ckphua</dc:creator>
    <dc:date>2016-10-07T21:30:53Z</dc:date>
    <item>
      <title>Bit band mapping on LPC5410x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604343#M23540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC5410x&lt;/P&gt;&lt;P&gt;There seems to be little info about using bit-banding on this device. Where can I find this information, for example mapping between the bit-band area and specific peripheral register bits? Which peripherals use bit-banding?......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 11:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604343#M23540</guid>
      <dc:creator>rogerlittlewood</dc:creator>
      <dc:date>2016-10-05T11:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: Bit band mapping on LPC5410x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604344#M23541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x&amp;nbsp;Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.&lt;/P&gt;&lt;P&gt;This means all the APB Peripherals are mapped in the bit-band region.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 21:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604344#M23541</guid>
      <dc:creator>ckphua</dc:creator>
      <dc:date>2016-10-07T21:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Bit band mapping on LPC5410x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604345#M23542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. So I hope the new version comes out soon so we can start to use those clever features thoughtfully provided by the ARM system designers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2016 07:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Bit-band-mapping-on-LPC5410x/m-p/604345#M23542</guid>
      <dc:creator>rogerlittlewood</dc:creator>
      <dc:date>2016-10-10T07:29:01Z</dc:date>
    </item>
  </channel>
</rss>