<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCXpresso OM13058 LPC11U68 VREFN maximum voltage? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-OM13058-LPC11U68-VREFN-maximum-voltage/m-p/604167#M23523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The set of the VREFP and VREFN should follow the rules:&lt;/P&gt;&lt;P&gt;1. The VREFP voltage level must be between 2.4 V and Vdda.&lt;/P&gt;&lt;P&gt;2. (VREFP-VREFN)/2 + VREFN = VDDA/2&lt;/P&gt;&lt;P&gt;Hole it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 06:05:16 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-09-13T06:05:16Z</dc:date>
    <item>
      <title>LPCXpresso OM13058 LPC11U68 VREFN maximum voltage?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-OM13058-LPC11U68-VREFN-maximum-voltage/m-p/604166#M23522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a specification for maximum VREFN voltage? In the datasheet and user manual there are recommendations for best performance, but no hard limits except for the upper limit on VREFP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the user manual, page 304 :&lt;/P&gt;&lt;P&gt;"Remark: For best performance, select VREFP and VREFN at the same voltage levels as VDDA and VSSA. When selecting VREFP and VREFN different from VDDA and VSSA , ensure that the voltage midpoints are the same:&lt;BR /&gt;(VREFP-VREFN)/2 + VREFN = VDDA/2"&lt;/P&gt;&lt;P&gt;I am attempting to set VREFN at approximately 2.7V and VREFP at approximately 3.2V, for about 0.5V difference, using LM385 voltage references. VREFP pin is fine, I can connect either reference to it, but with VREFN pin it is pulled down to 0.85V. I can't see anything on the OM13058 schematic to explain this so I am wondering if it some kind of internal protection in the MCU itself?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any experience trying to use a similar high VREFN voltage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 05:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-OM13058-LPC11U68-VREFN-maximum-voltage/m-p/604166#M23522</guid>
      <dc:creator>dirtyd</dc:creator>
      <dc:date>2016-09-09T05:09:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso OM13058 LPC11U68 VREFN maximum voltage?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-OM13058-LPC11U68-VREFN-maximum-voltage/m-p/604167#M23523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The set of the VREFP and VREFN should follow the rules:&lt;/P&gt;&lt;P&gt;1. The VREFP voltage level must be between 2.4 V and Vdda.&lt;/P&gt;&lt;P&gt;2. (VREFP-VREFN)/2 + VREFN = VDDA/2&lt;/P&gt;&lt;P&gt;Hole it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 06:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-OM13058-LPC11U68-VREFN-maximum-voltage/m-p/604167#M23523</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-13T06:05:16Z</dc:date>
    </item>
  </channel>
</rss>