<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC2103 GPIO pin High/Low in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2103-GPIO-pin-High-Low/m-p/603955#M23517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eshwar,&lt;/P&gt;&lt;P&gt;Have you ensured that the programmer was able to properly download the code? The proper registers for GPIO manipulation are explained on Chapter 8 “LPC2101/02/03 General Purpose Input/Output ports (GPIO)” of the “&lt;A href="http://www.nxp.com/documents/user_manual/UM10161.pdf"&gt;LPC2101/02/03 User manual&lt;/A&gt;”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also refer to the following GPIO tutorial for LPC2148:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.ocfreaks.com/lpc2148-gpio-programming-tutorial/"&gt;http://www.ocfreaks.com/lpc2148-gpio-programming-tutorial/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Oct 2016 04:16:23 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2016-10-06T04:16:23Z</dc:date>
    <item>
      <title>LPC2103 GPIO pin High/Low</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2103-GPIO-pin-High-Low/m-p/603954#M23516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am new to LPC2103. i bought this LPC2103 Controller for my project purpose.in this first i need to high/low the gpio pin.i saw the user manual provided in NXP.i saw the registers used for &amp;nbsp;GPIO. i used PINSEL,IODIR,IOCLR,IOSET registers.these registers are enough or any other registers are required for GPIO pin High/Low because i wrote the code using these registers and downloaded the code to micro controller through Python chip programmer.the code is downloaded but it is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please let me know what else are required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;Eshwar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 06:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2103-GPIO-pin-High-Low/m-p/603954#M23516</guid>
      <dc:creator>eswarchand</dc:creator>
      <dc:date>2016-10-04T06:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2103 GPIO pin High/Low</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2103-GPIO-pin-High-Low/m-p/603955#M23517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eshwar,&lt;/P&gt;&lt;P&gt;Have you ensured that the programmer was able to properly download the code? The proper registers for GPIO manipulation are explained on Chapter 8 “LPC2101/02/03 General Purpose Input/Output ports (GPIO)” of the “&lt;A href="http://www.nxp.com/documents/user_manual/UM10161.pdf"&gt;LPC2101/02/03 User manual&lt;/A&gt;”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also refer to the following GPIO tutorial for LPC2148:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.ocfreaks.com/lpc2148-gpio-programming-tutorial/"&gt;http://www.ocfreaks.com/lpc2148-gpio-programming-tutorial/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 04:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2103-GPIO-pin-High-Low/m-p/603955#M23517</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-10-06T04:16:23Z</dc:date>
    </item>
  </channel>
</rss>