<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there a command-line flash tool available for LPCXpresso54608? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-there-a-command-line-flash-tool-available-for-LPCXpresso54608/m-p/603892#M23511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For automatic tests purpose I'm looking for a tool able to flash a LPCXpresso54608 (precisely a OM13092 demo board). I used Flash Magic and the SEGGER J-Link software suite but the first can't write to the external Flash and the other brings up a pop-up each day that prevents the continuous testing process to run without a human action.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there currently a tool who:&lt;/P&gt;&lt;P&gt;- is able to program the external Flash,&lt;/P&gt;&lt;P&gt;- can be scripted in a command-line style,&lt;/P&gt;&lt;P&gt;- doesn't bring a pop-up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Apr 2017 07:21:12 GMT</pubDate>
    <dc:creator>bastienjauny</dc:creator>
    <dc:date>2017-04-12T07:21:12Z</dc:date>
    <item>
      <title>Is there a command-line flash tool available for LPCXpresso54608?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-there-a-command-line-flash-tool-available-for-LPCXpresso54608/m-p/603892#M23511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For automatic tests purpose I'm looking for a tool able to flash a LPCXpresso54608 (precisely a OM13092 demo board). I used Flash Magic and the SEGGER J-Link software suite but the first can't write to the external Flash and the other brings up a pop-up each day that prevents the continuous testing process to run without a human action.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there currently a tool who:&lt;/P&gt;&lt;P&gt;- is able to program the external Flash,&lt;/P&gt;&lt;P&gt;- can be scripted in a command-line style,&lt;/P&gt;&lt;P&gt;- doesn't bring a pop-up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 07:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-there-a-command-line-flash-tool-available-for-LPCXpresso54608/m-p/603892#M23511</guid>
      <dc:creator>bastienjauny</dc:creator>
      <dc:date>2017-04-12T07:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a command-line flash tool available for LPCXpresso54608?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-there-a-command-line-flash-tool-available-for-LPCXpresso54608/m-p/603893#M23512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MCUXpresso IDE provides a GUI flash programmer (and corresponding command line) that can do this via the built in&amp;nbsp;LPC-Link2 (with CMSIS-DAP firmware) on this board. See the MCUXpresso IDE User Guide for more details (available for download from &lt;A href="http://www.nxp.com/mcuxpresso/ide"&gt;http://www.nxp.com/mcuxpresso/ide&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 15:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-there-a-command-line-flash-tool-available-for-LPCXpresso54608/m-p/603893#M23512</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-12T15:34:56Z</dc:date>
    </item>
  </channel>
</rss>