<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Strange DMA Behaviour.Can someone help ???? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Strange-DMA-Behaviour-Can-someone-help/m-p/517755#M2331</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leonardo on Sat Jun 30 13:56:21 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi to forum &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I wish to transfer some data from an spi memory (at26df081) to the internal ram&amp;nbsp; of an LPC1754.I wish to use DMA in 16 bit mode which i found is the most efficient in terms of speed . I made the programming for the DMA controller and it works ok .After my first tests i show byte swapping since the writing is made in 8 bit mode.So i decided to use BIG endian mode transfer . Switching to big endian mode DMA fills the memory with zeros instead of my data . Has anybody noticed such a problem ?.Switching to little endian mode i see the data are correct but i must swap bytes .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas ?????.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:33:02 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:33:02Z</dc:date>
    <item>
      <title>Strange DMA Behaviour.Can someone help ????</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Strange-DMA-Behaviour-Can-someone-help/m-p/517755#M2331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leonardo on Sat Jun 30 13:56:21 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi to forum &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I wish to transfer some data from an spi memory (at26df081) to the internal ram&amp;nbsp; of an LPC1754.I wish to use DMA in 16 bit mode which i found is the most efficient in terms of speed . I made the programming for the DMA controller and it works ok .After my first tests i show byte swapping since the writing is made in 8 bit mode.So i decided to use BIG endian mode transfer . Switching to big endian mode DMA fills the memory with zeros instead of my data . Has anybody noticed such a problem ?.Switching to little endian mode i see the data are correct but i must swap bytes .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas ?????.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Strange-DMA-Behaviour-Can-someone-help/m-p/517755#M2331</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: Strange DMA Behaviour.Can someone help ????</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Strange-DMA-Behaviour-Can-someone-help/m-p/517756#M2332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdurand on Sat Jun 30 19:10:44 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I haven't tried it, but since this is a 32 bit part, could you be swapping the upper 16 bits down to the lower 16 bits?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Strange-DMA-Behaviour-Can-someone-help/m-p/517756#M2332</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:33:03Z</dc:date>
    </item>
  </channel>
</rss>