<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: ADC PCLK for LPC1114fn28/102</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600373#M23294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As stated on Users's Manual (ADC chapter):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The APB clock (PCLK) is divided by CLKDIV +1 to produce the clock for the ADC, which&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;should be less than or equal to 4.5 MHz. Typically, software should program the smallest&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;value in this field that yields a clock of 4.5 MHz or slightly less, but in certain cases (such&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;as a high-impedance analog source) a slower clock may be desirable."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum PCLK is around 48 MHz (the exact value depends on your specific setup and clock source, PLL, interrnal RC oscillator,...).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 00:43:33 GMT</pubDate>
    <dc:creator>dirceurodrigues</dc:creator>
    <dc:date>2017-02-06T00:43:33Z</dc:date>
    <item>
      <title>ADC PCLK for LPC1114fn28/102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600372#M23293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My friend and I cannot seem to find a solid answer, neither through the user manual nor the datasheet. &amp;nbsp;What is the frequency of the PCLK for the ADC block on the LPC1114fn28/102? &amp;nbsp;The more information the better!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you :smileyhappy:&lt;/P&gt;&lt;P&gt;Austin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 17:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600372#M23293</guid>
      <dc:creator>austinpalanca</dc:creator>
      <dc:date>2017-02-03T17:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: ADC PCLK for LPC1114fn28/102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600373#M23294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As stated on Users's Manual (ADC chapter):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The APB clock (PCLK) is divided by CLKDIV +1 to produce the clock for the ADC, which&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;should be less than or equal to 4.5 MHz. Typically, software should program the smallest&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;value in this field that yields a clock of 4.5 MHz or slightly less, but in certain cases (such&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;as a high-impedance analog source) a slower clock may be desirable."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum PCLK is around 48 MHz (the exact value depends on your specific setup and clock source, PLL, interrnal RC oscillator,...).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 00:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600373#M23294</guid>
      <dc:creator>dirceurodrigues</dc:creator>
      <dc:date>2017-02-06T00:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: ADC PCLK for LPC1114fn28/102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600374#M23295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much! &amp;nbsp;We are going to use the IRC (by default) which operates at about 12 Mhz, then divide it twice, once from PLL and once with the ADC clkdiv to achieve our results.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 18:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-PCLK-for-LPC1114fn28-102/m-p/600374#M23295</guid>
      <dc:creator>austinpalanca</dc:creator>
      <dc:date>2017-02-06T18:56:04Z</dc:date>
    </item>
  </channel>
</rss>