<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How many PWM channels with LPC1769? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PWM-channels-with-LPC1769/m-p/517731#M2327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Paul on Mon Sep 30 11:37:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You can use the following peripherals in the LPC1769 to create PWMs:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM block - up to 6 single-edge or 3 double-edge controlled PWMs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Motor Control PWM - has three PWM channels&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Timers 0/1/2/3 - each of these timers can be used as three PWM channels&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:30:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:30:57Z</dc:date>
    <item>
      <title>How many PWM channels with LPC1769?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PWM-channels-with-LPC1769/m-p/517730#M2326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by motumboe on Mon Sep 30 10:04:59 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am going to select an LPCxxxx microcontroller for an application with 8 (9 would be better) PWMs that I need to run at 20 kHz and 4 PWMs at 1 kHz. I also need other 2 slower PWMs but I can do a software PWM for them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also need at least 256 kb Flash. The parametric search tells me that I have only 6 PWMs on the LPC1769. Is it true? Is there a way to get more PWMs out of this microcontroller?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and sorry for the silly question.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; Marco&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PWM-channels-with-LPC1769/m-p/517730#M2326</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: How many PWM channels with LPC1769?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PWM-channels-with-LPC1769/m-p/517731#M2327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Paul on Mon Sep 30 11:37:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You can use the following peripherals in the LPC1769 to create PWMs:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PWM block - up to 6 single-edge or 3 double-edge controlled PWMs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Motor Control PWM - has three PWM channels&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Timers 0/1/2/3 - each of these timers can be used as three PWM channels&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PWM-channels-with-LPC1769/m-p/517731#M2327</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:30:57Z</dc:date>
    </item>
  </channel>
</rss>