<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1875 SDRAM Reading infinitely;CPU locked up in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1875-SDRAM-Reading-infinitely-CPU-locked-up/m-p/600143#M23269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a custom board which uses LPC1857 cortex-M3 processor. The SDRAM&amp;nbsp;AS4C16M16SA (4M word x 16-bit x 4-bank) connected to DYCS1. The SDRAM initliazation looks ok on the scope. Also SDRAM write seems to be ok. Below in the SDRAM/Controller configuration and intialization code attached.&amp;nbsp;&lt;/P&gt;&lt;P&gt;While reading a byte until address 0x30000000 to 0x30000003 everything seems ok and I think it is because of the buffer. After that porocessor locks up and goes for infinite read. I would appreciate if anybody could help with their ideas.&amp;nbsp;&lt;/P&gt;&lt;P&gt;testing method:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;#define SDRAM_BASE_ADDR (0x30000000 | 0x3)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&amp;nbsp;//write&lt;BR /&gt; &amp;nbsp;&amp;nbsp;add = (uint8_t *)(SDRAM_BASE_ADDR );&lt;BR /&gt; &amp;nbsp;&amp;nbsp;for (i=0;i&amp;lt;66;i++)&lt;BR /&gt; &amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;*add = num1 ;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;//num1++;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;add++;&lt;BR /&gt; &amp;nbsp;&lt;BR /&gt; &amp;nbsp;}&lt;BR /&gt; &amp;nbsp; blink(led1);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt; &amp;nbsp; //read&lt;BR /&gt; &amp;nbsp;&amp;nbsp; add = (uint8_t *)(SDRAM_BASE_ADDR );&lt;BR /&gt; &amp;nbsp;&amp;nbsp;for (i=0;i&amp;lt;1i++)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;val1[i] = *add;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;add++;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;}&lt;BR /&gt; &amp;nbsp; while (1) {blink(led2);}&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;-Using Keil MDK Pro and Jlink debug adapter&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;Sanjay&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338009"&gt;sdram-init.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 15:01:36 GMT</pubDate>
    <dc:creator>sanjaymurthy</dc:creator>
    <dc:date>2017-02-03T15:01:36Z</dc:date>
    <item>
      <title>LPC1875 SDRAM Reading infinitely;CPU locked up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1875-SDRAM-Reading-infinitely-CPU-locked-up/m-p/600143#M23269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a custom board which uses LPC1857 cortex-M3 processor. The SDRAM&amp;nbsp;AS4C16M16SA (4M word x 16-bit x 4-bank) connected to DYCS1. The SDRAM initliazation looks ok on the scope. Also SDRAM write seems to be ok. Below in the SDRAM/Controller configuration and intialization code attached.&amp;nbsp;&lt;/P&gt;&lt;P&gt;While reading a byte until address 0x30000000 to 0x30000003 everything seems ok and I think it is because of the buffer. After that porocessor locks up and goes for infinite read. I would appreciate if anybody could help with their ideas.&amp;nbsp;&lt;/P&gt;&lt;P&gt;testing method:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;#define SDRAM_BASE_ADDR (0x30000000 | 0x3)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&amp;nbsp;//write&lt;BR /&gt; &amp;nbsp;&amp;nbsp;add = (uint8_t *)(SDRAM_BASE_ADDR );&lt;BR /&gt; &amp;nbsp;&amp;nbsp;for (i=0;i&amp;lt;66;i++)&lt;BR /&gt; &amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;*add = num1 ;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;//num1++;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;add++;&lt;BR /&gt; &amp;nbsp;&lt;BR /&gt; &amp;nbsp;}&lt;BR /&gt; &amp;nbsp; blink(led1);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt; &amp;nbsp; //read&lt;BR /&gt; &amp;nbsp;&amp;nbsp; add = (uint8_t *)(SDRAM_BASE_ADDR );&lt;BR /&gt; &amp;nbsp;&amp;nbsp;for (i=0;i&amp;lt;1i++)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;val1[i] = *add;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;add++;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;}&lt;BR /&gt; &amp;nbsp; while (1) {blink(led2);}&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;-Using Keil MDK Pro and Jlink debug adapter&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="color: black;"&gt;Sanjay&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; background: white;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338009"&gt;sdram-init.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 15:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1875-SDRAM-Reading-infinitely-CPU-locked-up/m-p/600143#M23269</guid>
      <dc:creator>sanjaymurthy</dc:creator>
      <dc:date>2017-02-03T15:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1875 SDRAM Reading infinitely;CPU locked up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1875-SDRAM-Reading-infinitely-CPU-locked-up/m-p/600144#M23270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just in case if anyone come around this problem it was the clock. I had configured just Clk1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sanjay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 12:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1875-SDRAM-Reading-infinitely-CPU-locked-up/m-p/600144#M23270</guid>
      <dc:creator>sanjaymurthy</dc:creator>
      <dc:date>2017-02-07T12:33:23Z</dc:date>
    </item>
  </channel>
</rss>